Motor Replacement Kit Zoom

Motor Replacement Kit

SKU:MRK

Brand: EWC Controls

EWC Controls
Qty Price
$73.95
/ each
In Stock! Ships in 24-48 Hours
(2 Available)
0

Resources

Specs

Product Type: Motor Kit
Application: Motor Replacement for EWC Damper Motors

Description for EWC Controls MRK

Motor replacement kit used for all styles of ND - URD and RDN dampers.

Motor Replacement Kit

REVIEW SNAPSHOT®

by PowerReviews
EWC ControlsMotor Replacement Kit
 
4.9

(based on 15 reviews)

Ratings Distribution

  • 5 Stars

     

    (14)

  • 4 Stars

     

    (1)

  • 3 Stars

     

    (0)

  • 2 Stars

     

    (0)

  • 1 Stars

     

    (0)

100%

of respondents would recommend this to a friend.

Pros

    Cons

      Best Uses

          • Was this a gift?:
          • No (3)

        Reviewed by 15 customers

        Sort by

        Displaying reviews 1-10

        Back to top

        Previous | Next »

         
        5.0

        Fast shipping and Great price

        By MRAGS

        from Connecticut

        Verified Buyer

        Pros

          Cons

            Best Uses

              Comments about Motor Replacement Kit:

              The MA-ND5 is an upgrade actuator over the MA-ND3 that were origional equipment on my duct work. I'm very satified with the ease of installation and knowing I've purchased a newer /upgraded version damper motor at a terrific price, thanks again Pexsupply for a nice buying experience without any B/S

              • Was this a gift?:
              • No
               
              5.0

              I would buy this product again

              By Mg

              from Connecticut

              Verified Buyer

              Pros

                Cons

                  Best Uses

                    Comments about Motor Replacement Kit:

                    Great service

                    • Was this a gift?:
                    • No
                     
                    5.0

                    Not mechanically inclined? No worries!

                    By DaveyBob

                    from Atlanta, GA

                    Verified Buyer

                    Pros

                      Cons

                        Best Uses

                          Comments about Motor Replacement Kit:

                          I'm reasonably good with pliers and a screwdriver, but I'm no engineer. I had no problem at all replacing the old motor on my damper. Just be sure you orient the damper position correctly before locking it down. The red/green lights to show closed/open are good.

                          • Was this a gift?:
                          • No
                           
                          5.0

                          Perfect

                          By Mo

                          from Blue Springs MO

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          Replacement for a 3 series motor, exact fit - easy instalation. Didn't need any of the brackets or screws. Con - did not include a damper position indicator, the old 3 series one did not adapt.

                           
                          5.0

                          Great Experience.

                          By John

                          from New Freedom PA

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          The part ordered from Pex came very quickly, was packaged safely, and there were no problems at all with the order. I would definitely order from Pex Supply again. Great experience overall.

                           
                          5.0

                          Works with Honeywell EnviraZone Panel

                          By RjinTX

                          from Houston, TX

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          I replaced my Carrier WeatherMaker zone controller with a Honeywell EnviraZone panel. Those damper motors were relying on the Carrier zone controller to turn them on/off, so they kept running non-stop since they Honeywell doesn't work that way. They are also motor open/close (no springs). I replaced them with these damper motors and they work great with the Honeywell panel. They also allow the zone ON/OFF lights to work correctly on the Honeywell panel. A nice touch to also have the red and green LED lights on the motors to indicate if they are in the open or closed position. They installed right over the existing damper knob and I tightened them securely. They were easy to install and were fully adjustable for their open/close distance.

                           
                          5.0

                          Excellent

                          By MikeJones

                          from Louisiana

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          Great service from PEX, and great product fit for ND3 replacement. Ten mins to replace, and the new unit seems to have quite a few updates since the ND3.

                           
                          5.0

                          Easy DIY Project

                          By DIY Enthusiast

                          from Denville, NJ

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          I ordered 2 MRK units to replace EWC Controls Inc. MA-ND3 damper motors that had stopped functioning. It took about 20 minutes to replace both units. You need only to disconnect three wires from the old units and then remove the old units from the damper per the accompanying instructions. The MRKs are then reattached in the same manner. Just make sure to label the wires so you hook them back up to the correct terminals. Also make sure when you attach the motor to the damper actuator that the damper and the actuator clamp are both oriented to the open position.

                          This was one project that is as easy to accomplish as you think it should be.

                           
                          4.0

                          Easy installation

                          By CTVince

                          from Connecticut

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          Used to replace MA-ND3 damper motors in residential application. Easy installation and the directions were fairly easy to follow. Only gave 4 stars because they have only been installed for about 3 wks. We'll see if they perform for the long term.

                           
                          5.0

                          Working great!

                          By Heath

                          from SC

                          Verified Buyer

                          Comments about Motor Replacement Kit:

                          I used these to replace the Carrier Comfortmaker actuators installed in my house in 1997. These actuators are working great! I had to reposition the old rear mount that was already in place on my dampers - but it all worked out in the end.

                          Displaying reviews 1-10

                          Back to top

                          Previous | Next »

                          Q&A: Ask the Questions, share answers

                          Do you have questions about this product?

                          get answers from real customers and in-house experts with AnswerBox.

                          1 Question | 1 Answer
                          Displaying question 1
                          • Motor Replacement Kit

                            Q:

                            Our damper won't close, will replacing it with this motor fix that problem for us? Is this the right part? the only part we'll need to be able to have the damper open and close?
                            Asked on 8/8/2013 by Ashley

                            1 answer

                            • VERIFIED BUYER

                              A:

                              It did for me!
                              My original circuit board / motor assembly was a model MA-ND3. I was told by the manufacturer EWC in Englishtown, NJ that the Model MRK was the universal replacement Motor / Board for EWC Controls UltraZone Damper motors.
                              And it was. I replaced two of them already: The first in 2007, was a direct fit. The second damper was smaller than the length of the replacement Motor / Board - so I had to customize it a bit. The MRK comes with an extra mounting plate and screws - so with a pair of pliers it really was not difficult. I really love the quality of the EWC products; and PEX Supply.
                              Good Luck.

                              Answered on 8/8/2013 by BobM from Pottstown, PA
                          Displaying question 1

                          Do you have a question about this product?