Choosing the bathtub that will work perfectly in your bathroom is not an easy
decision. There are many different things that one must consider. The
information below is provided to help you pick out a perfect bathtub for your
particular tastes!
Corner Tub Corner tubs are usually installed without integrated showers. Corner tubs are usually available in 5' or 6' lengths. They tend to use a lot of floor space, however, so they're not suitable for all bathrooms. Corner baths can have drains on either side or in the middle, and some models are not suitable for an overhead shower.
3 Wall Alcove / Recess Tub Also referred to as recessed tubs, 3 wall alcove tubs are the most popular style in this product category. The tub is installed against three walls, and thus, only shows one side with a decorative finish.
Drop In / Sunken Tub Drop in tubs are usually mounted on a platform and have visible rims. They require a platform on which the tub rests.
Undermount Tub This type of tub is usually mounted on a platform. It has no visible sides.
Clawfoot / Free Standing Tub These tubs are typically built with four legs so that they stand freely. They are not installed against walls or mounted on a platform, and thus, all sides of the tub are visible. This is a popular selection for families who are seeking a traditional, antique or vintage style tub.
Pedestal / Free Standing Tub Pedestal tubs have an oval shape, and rest on an oval base. These tubs offer better weight distribution without the hassle of cleaning under them. Faucets can be either floor or wall mounted
Slipper / Free Standing Tub Slipper tubs are cast iron tubs with extended backs.
Soaking Tub These oversized tubs provide for total immersion. The tub within a tub allows a continuous, gentle cascade of water to overflow the sides and produce a relaxing visual and aural sensation, while softly floating the user's body. The bather stays warmer than in traditional baths as the shoulders and torso can be completely submerged. Their extra length provide for comfortable support and natural leg extension.
Greek Bath Greek baths provide a space saving alternative to the usual soaking tub. Designed for one person bathing, their space-saving sizes have an extra deep basin for soaking. These tubs can be installed in a 3-wall alcove or as a drop-in.
Drain Location
To purchase the correct bathtub, you must know where the drain should be. To figure this out, the following rules apply:
End Drain Tub - If you face the tub and the drain is on the right side, you need a right hand tub. Similarly, if you face the tub and the drain is on the left side, you need a left hand tub.
Center Drain Tub In some cases, the drain will be located in the center of the tub.
Some drains are reversible, which means you can turn the bathtub to face either side - thus the location of the drain won't matter.
Size
Rectangular, Oval, and Round shaped tubs are all measured in the same way. The three important measurements are length, width, and height. Be sure to have a good idea of how much room you have in your bathroom. You want to be certain that even with the tub installed, you will be able to walk around with ease. As a general rule, there should be at a minimum 60"(L) x 30" (W) of open space immediately in front of the bathtub. \
Shape
Shape is typically a matter of personal preference. We strive to provide you with the largest selection of bathtubs in the industry. Bathtubs are available in the following shapes:
Color
Most bathtubs come in a variety of colors to match your bathroom d้cor. This being said, different manufacturers tend to supply different colors. Some of the finishes that bathtubs are available in are as follows:
Black
Neutrals
Shades of Blue
Shades of Grey
Shades of Red
White
Materials (Show me examples!)
The two most popular materials are acrylic and cast iron. While Acrylic is cheaper, lighter, and sometimes easier to install, we recommend cast iron more because it keeps the heat in better, lasts longer, is more durable, deadens the splashing sounds of the water, and actually feels better on your feet. Below is a more extensive description of both.
Fiberglass Gel-coated fiberglass is generally the least expensive material for bathtubs. It is lightweight, easy to install, and can be molded into a variety of shapes. The gel-coat surface is thinner and less durable than acrylic. While the finish won't last as long as other materials (it shows wear after 10 to 15 years), and can scratch or fade, it is also easily repaired. Fiberglass units can be cleaned with a mild detergent such as dishwashing soap.
Acrylic Inexpensive material is shiny and can be decorative. It is resistant to cracking, chipping, peeling, and staining. The color runs through the entire tub and will not fade. Acrylic is easy to sanitize with common non-abrasive cleaners and water. Acrylic tubs are available in most colors and shapes. An acrylic tub is adequate, although cast iron will keep heat in longer and will reduce the noise of running water.
Cast Iron The strongest material available for a bathtub. The benefits of cast iron are that it keeps heat in longer, will usually last a lifetime (very durable), will deaden the splashing water sound well, and usually feels better on your feet. The negatives are that it sometimes requires additional structural support in the floor below, can be susceptible to chips (rarely), and is more expensive than acrylic. Cast Iron tubs are available in a variety of colors and shapes.
For Phone Sales please call 1-516-749-6375.
We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
We carry all products from the brands you see on our website plus we also carry more brands not listed online. For
sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open
from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or,
contact us via email!