MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
Getting rid of food waste can be one of the most laborious and smelly chores in the world. Luckily for you, it doesn’t have to be that way. Investing in a garbage disposer will be one of the best decisions you make for your kitchen. So be smart, and don’t cut corners where going the extra yard can make all the difference in the world.

What Does a Disposer Do?
  • Provides you with faster meal preparation and cleanup
  • Helps to sanitize your kitchen sink area
  • Decreases the amount of garbage that you need to bag
  • Because less garbage is bagged, you help to keep the environment cleaner
  • No bad food odor in garbage

    Continuous Feed vs. Batch Feed
  • Continuous Feed: Most disposers are continuous feed and manually controlled by a wall or sink-top switch. This helps to keep hands clear of the disposer when it’s turned on. While operating, the mouth of the unit remains open and is protected by a rubber anti-splash baffle. This permits you to continuously feed waste into the grinder. However, the baffle will wear, and thus must occasionally be replaced.
  • Batch Feed: A Bath feed disposer is a safer model that only functions when the stopper is placed into the drain. This keeps the mouth of the unit closed off while operating and in turn prevents you from grinding your hands by accident. Because no wall or sink-top switch is needed, installation will also be easier. However, you can't continually feed waste into the disposer of a batch feed model. Only the "batch" already under the stopper can be disposed of at a given time. Despite this limitation, which only comes into effect if you need to process large amounts of waste, we strongly suggest installing a batch feed disposer. For only a slight increase in price, you can help guarantee the safety of yourself and children. This notion has already started to catch on in the Northeastern states, and it's time for the rest of the world to realize it as well.

     Back to top or find a garbage disposal

    Features To Consider
  • Horsepower: Disposers with the most power will operate the quickest and most effectively. It is generally acknowledged that motors with up to 1 hp are suitable for use in residential homes.
  • Noise Reduction: While speed and power are positive features in a disposer, operating noise can be very annoying. You can moderate operating noise through the use of induction motors and insulated grind chambers.
  • Components (Material): Stainless steel and chrome are the strongest materials and will enable disposers to last for years.
  • Warranties: Every Company offers a unique warranty. Typically, the bigger and more powerful the model, the longer it will be. Be confident in your selection – make sure the manufacturer stands behind their products.

    What you should do
  • Throw away food scraps into the disposer, not the garbage.
  • Make sure to run cold water into the disposer if you are disposing small amounts of fats and greases.
  • Use your disposer to grind all hard materials (Ex. chicken bones)
  • Peel citrus fruits and process the rind to freshen the drain.

    What you should not do
  • Do not use hot water when grinding food waste.
  • Do not stop running cold water into the disposer until you have finished grinding the waste.
  • Do not turn off the disposer in the middle of operation.
  • Do not put glass or metal (eating utensils) into the disposer.
  • DO NOT PUT YOUR HANDS INTO THE CHAMBER.
  • Avoid grinding high-fiber materials (Ex. Corn husks)

     Back to top or find a garbage disposal

    * These tips are meant as a helpful resource. SupplyHouse.com strongly suggests consulting a licensed contractor and referencing the manufacturer's instructions.

    continous feed
    batch feed



    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan