MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
Introduce color and style to your bathroom with a new lavatory faucet. “Lavatory” is the industry term for a bathroom or washroom sink. A lavatory faucet is a type of faucet designed to deliver water into a lavatory. If you’re looking for a change in your bathroom…something new…you'll be delighted with the faucets that are available today. Here’s how to educate yourself so that the faucet you choose is perfect in every way:
  • Color finish
  • Handle type
  • Spout types
  • Faucet configuration
  • Faucet construction
  • Accessories

    Color Finish
    Most faucets come in a variety of colors to match your bathroom decor. Interestingly, while chrome is the most durable, it's also the most affordable. Alternative coatings are substantially more expensive. Different manufacturers tend to supply different finishes and colors. Some of the finishes that lavatory faucets are available in are as follows:
  • Polished Chrome
  • Polished Brass
  • Colored epoxy (glacier white, almond, biscuit, and black)
  • Polished nickel
  • Satin nickel
  • Stainless Steel
  • Bronze
  • Gold
  • Porcelain (some porcelain is even being hand-painted now!)

    Handle type  (Show me examples!)
    Select a handle type that will compliment your bathroom. Faucets traditionally come with two handles. One is for hot water and one is for cold water. This gives you independent control of both handles. When using a two-handle faucet, remember that cross-handles and lever handles provide an easy grip. Lavatory faucets are now available in single-handle versions. Single-handle, or "single control" faucets give you the convenience of being able to control the water temperature and pressure with one single control.

     Back to top or find a lavatory faucet now

    Spout types  (Show me examples!)
    The type of spout you are going to choose is simply personal preference. Most basic lavatory faucets will have standard spouts. High-arc spouts are becoming more popular on lavatory faucets. If you are planning to wash your hair in the bathroom sink, you may want to consider a lavatory faucet with a high-arc spout. Manufacturers are making their spouts longer and more decorative than ever before, so your lavatory faucet can stand out in your bathroom.

    Faucet Configuration  (Show me examples!)
    When purchasing a deck-mount faucet (a faucet that mounts on the lavatory sink or deck) you must choose a faucet that will fit your lavatory sink. If you don’t match the configuration of the lavatory faucet with the lavatory sink, chances are it won’t fit! In fact, most plumbers will not drill an additional hole in a lavatory sink because the sink will most likely crack. The three configurations of a lavatory faucet are single-hole, centerset, and widespread.
  • Single-hole – requires one hole drilling in the sink
  • Centerset – the hole drillings for the hot and cold handle are 4” apart
  • Widespread – the hole drillings for the hot and cold handle are 8” –16” apart

     Back to top or find a lavatory faucet now

    Although deck-mount faucets are most common, more and more people are considering wall-mount faucets. Instead of mounting on the sink itself, a wall-mount faucet mounts on the wall above the sink.

    Faucet Construction
    The construction of the faucet is important because you may be able to save money on a cheap faucet now, but you’ll be paying the difference in repair or replacement costs later. Your options for the faucet’s construction material come down to solid brass or plastic. Brass is by far the most recommended choice because of its toughness and ability to handle extreme temperatures.

    Internally, your faucet will control the flow of water using either rubber washers, a plastic or ceramic cartridge, a plastic, brass, or stainless steel ball valve, or a ceramic disk. Ceramic cartridges allow the handles to open and close at precisely the same spot every time. Alternately, a ball valve uses washers, which wear out and require you to continually adjust the handle position. A ceramic disk is highly recommended.

    Accessories  (Show me examples!)
  • Rough-in Valves - Be careful! Some manufacturers sell the lavatory faucet trim separate from the rough-in valve unit that actually makes the faucet function.
  • Handles and accents - Some manufacturers sell the handles and the handle accents separate from the faucet. This is done so that the customer can mix and match finishes creating the faucet of their dreams.
  • Drains - If you were thinking you would have to purchase the drain for your lavatory faucet separately, you’re wrong! Most lavatory faucets include the drain!

     Back to top or find a lavatory faucet now

    single handle
    two handle
    high arc
    wall mount
    single hole
    centerset
    widespread
    rough in valve
    handles & accents
    drains



    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan