MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
If you’re in the process of renovating your bathroom, don’t forget to purchase a brand new shower receptor. When making such a selection, there are many important things that one must consider. The information below is provided to answer any questions you may have along the purchasing process.
  • Shape
  • Threshold
  • Size
  • Color
  • Drain finish

    Shape
    Shape is typically a matter of personal preference. We strive to provide you with the largest selection of shower receptors in the industry. Shower receptors are available in the following shapes:
  • Neo-angle*
  • Rectangle
  • Round
  • Square
    * If you wish to save space and install the receptor in a corner, the neo-angle base is the optimal choice. Out of all of the shower receptors, it takes up the least amount of floor space and can still help any bathroom design be exquisite.

     Back to top or find a shower receptor now

    Threshold  (Show me examples!)
    When choosing between shower receptors, you should consider where you want to install the base. For example, will you place it against two walls, three walls….etc?? This will help you determine the threshold you need. Threshold refers to the amount of different entry points you can select for your base. The higher the threshold, the more options you will have when selecting a shower door. I know this is confusing!! Perhaps the more extensive explanation of threshold below will help clear this up.
  • Single Threshold: You should choose a single threshold shower receptor if you are going to install the base against three walls. This is because you only need a receptor with one point of entry.
  • Double Threshold: You should choose a double threshold shower receptor if you are going to install the base against two walls. One threshold should be fitted with a decorative enclosure and the other will serve as the entrance to the shower.
  • Triple Threshold: You choose a triple threshold shower receptor if you are going to install the base against only one wall. Two thresholds should be fitted with decorative enclosures and the third will serve as the entrance to the shower.

    Size
    Regardless of the shape of the shower receptor you choose, most bases are measured in the same way. The two important measurements are length and width. Generally, any shower base with dimensions at least 34” (L) X 34” (W) will be comfortable to use. However, be sure to have a good idea of how much room you have in your bathroom. The walls must be large enough to support the base, and be certain that even with the receptor installed you will be able to walk around with ease. As a general rule, there should be at a minimum 60"(L) x 30" (W) of open space immediately in front of the receptor.

     Back to top or find a shower receptor now

    Color
    Most shower receptors come in a variety of colors to match your bathroom décor. This being said, different manufacturers tend to supply different colors. Some of the finishes that receptors are available in are as follows:
  • Black
  • Neutrals
  • Shades of Blue
  • Shades of Green
  • Shades of Grey
  • Shades of Red
  • Whites

    Drain Finish  (Show me examples!)

    The last thing you need to decide before ordering a shower base is what kind of drain you want. We recommend that you choose the drain that will best complement the color of the receptor and faucets in your bathroom. Several popular drain finishes are:
  • Polished Brass
  • Brushed Nickel
  • Copper
  • Gold
  • Plastic

     Back to top or find a shower receptor now

    neo-angle
    rectangle
    square
    single threshold
    double threshold
    triple threshold
    polished brass
    brushed nickel



    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan