MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
Many things must be considered before purchasing the toilet that will work best in your bathroom. This article is provided to guide you along this selection process. So flush away your worries….everything you need to know is right below:
  • Rough-In
  • Bowl Shape
  • Flush Type
  • Wall Mount Toilets
  • Configuration
  • Height
  • Colors
  • Trip Levers

    Rough-In
    Rough-in refers to the space between the center of the toilet’s drain and the wall in back of the toilet. The standard distance between these two objects is 12,” but 10” and 14” are popular as well. When making your selection, you should keep the size of your bathroom in mind. As a general rule, you should maintain 16” of space from the centerline of the toilet to a lateral obstruction and at least 48” (L) X 48” (W) of open space in front of the toilet.

    Bowl Shape  (Show me examples!)

  • Round: A round bowl is smaller, and hence, requires less space than an elongated bowl. It stretches 16 ½” from the front of the bowl to the bolt holes in the back of the seat. The smaller size of the bowl makes it cheaper than an elongated bowl, but also a less comfortable option. A round bowl should only really be selected for the bathroom of children or if space necessitates such a choice.
  • Elongated: An elongated bowl is larger, and hence, requires more space than a round bowl. It stretches 18 ½” from the front of the bowl to the bolt holes in the back of the seat. It is slightly more expensive than a round bowl, but its stretched out shape makes it easier to use for adults. The water in the bowl also covers a larger surface area than in a round bowl.
  • Compact Elongated: A compact elongated toilet (available through Kohler) is a one-piece toilet that is designed to enable an elongated bowl to fit in a round-front space. This toilet saves on space while giving the same comfort as an elongated toilet.

     Back to top or find a toilet now

    Flush Type
    Traditional toilets had the luxury of operating at a water volume of 3 ½ - 7 gallons per flush. Today, however, our desire to save water has led to the creation of laws that only permits toilets to flush at a maximum rate of 1.6 gallons per flush. This has changed the effectiveness of flushing mechanisms, and makes choosing between flush types an important decision. Below is a description of the two most popular flush types, gravity fed and pressure assisted:
  • Gravity Fed Flush: This was the most effective option with older toilets, but it does not function as well with the new limitations on water usage. Gravity Flush toilets are more subject to clogging, and also do not clean the rims of the bowls as well as they used to.
  • Pressure Assisted Flush: Because of the limitations on water usage, Pressure Assisted toilets have become increasingly popular. They very rarely clog and are very good at cleaning themselves. Accordingly, they usually demand higher ticket prices than gravity fed toilets. A drawback is that pressure assisted toilets tend to produce higher operating noise than gravity fed toilets, and some of them must be plugged into electrical sockets.

    Kohler distinguishes itself from other manufacturers by offering the Peacekeeper and Power Lite series of pressure assisted toilets. The Peacekeeper Series toilet runs on battery power, so it does not require an electrical socket. They are designed to flush only when the user closes the lid, solving the age-old dispute over leaving the toilet seat up. The Power Lite series has a flush button and requires a socket.

    Wall Mount Toilets
    Wall mount toilets have become popular toilets recently because they save on space and are still stylish. A wall mount toilet eliminates the toilet base and this makes cleaning underneath the toilet quick and easy!

    Wall mount toilets are supported from the wall; this makes it possible to conceal all of the pipe connections and reduces the noise that is usually transferred through the floor when the toilet flushes. When installing your wall mount toilet it is important to decide whether you want a concealed tank or an exposed tank. A concealed tank is a tank that is hidden inside of the wall and a flush actuator is used (show me examples!) to flush the toilet. The exposed tank is a tank that is visible, similar to the tank on a regular toilet.

    When trying to determine the height requirements for the installation of the toilet, it is important to remember that most toilets are 16” to 17” from the floor to the rim of the bowl.

    Configuration  (Show me examples!)

    Toilets are available in both a one and two-piece construction. In a one-piece toilet, the tank is connected to the bowl. In a two-piece toilet, the tank and bowl are two distinct units that can be separated.

    One-piece toilets offer a more contemporary look than a two-piece toilet. Furthermore, because there is no crevice between the tank and the bowl, odorous substance will not accumulate. This sanitary feature of a one-piece toilet tends to make it slightly more expensive than a two-piece toilet. In addition, most one-piece toilets include the seat, but two-piece toilets do not. You should read the product descriptions carefully to make sure whether the seat is or is not included.

    *** If you purchase a two-piece toilet, you should consider buying an optional insulated tank. Built with a rubber coating inside, this tank will better prevent sweating from occurring (condensation).

    Height
    Although there is no standard height for toilets, most styles usually range from about 14.5 inches to 17 inches high. The 17” versions are made for ADA compliance. Yet, as a guideline to choosing the toilet that will best suite your needs, it is important to keep in mind two types of heights.

    Comfort Height - These toilets are comparable to the height of an average household chair, which makes sitting down and standing up easier. At a little over 17” these toilets maximize comfort.

    Family Height - These toilets offer a standard height between 15” and 16”, and are ideal for bathrooms that are used by everyone, especially children.



     Back to top or find a toilet now

    Colors
    Most toilets come in a variety of colors to match your bathroom décor. This being said, different manufacturers tend to supply different colors. Some of the finishes that toilets are available in are as follows:
  • Black
  • Neutrals
  • Blue
  • Red
  • Green
  • Grey
  • Whites

    Trip Levers  (Show me examples!)

    The trip lever, in a sense, is the “faucet” of the toilet. Accordingly, some people like to select a lever that matches the faucets on their tub and sink. Usually, the trip lever that comes with the toilet will match the color of the toilet or will be finished in polish chrome. However, below is a list of several other options:
  • Polished Brass
  • Brushed Nickel
  • Porcelain
  • Wood

     Back to top or find a toilet now

    round
    elongated
    gravity fed flush
    one piece
    two piece
    polished brass
    brushed nickel



    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan