Economical, efficient, elegant and stylish a Towel Warmer will add to the comfort of any room as well as keep your towels warm and dry. There is a wide range of standard units of different designs. To find the right towel warmer that will fit your household needs it is important to consider…
Benefits
For dry and fresh towels, after using your towel, fold it to double thickness. The next time you reach for your towel it will be dry and warm. Even in the humid summer months using a towel warmer will keep towels dry and stop them from smelling musty.
Also use a towel warmer to help dry cold damp winter clothes. Try putting your coats, jackets and mittens on the towel warmer. Not only will they dry and stay free of mildew, but they will also be nice and warm next time you want to put them on. Towel warmers can also dry, bathing suits and dry hand washables (e.g. sweaters) and other delicate laundry items that can't be tumble dried.
Heating types
Electronic
-
An electronic towel warmer is often the right choice for remodeling or where the entire space relies on electric heat.
Hydronic
-
Homes that use forced hot water and have proper plumbing access will find hydronic styles to be the most compatible. Even domestic hot water sources may be used under certain circumstances.
Wall-Mount -
A wall mount towel warmer can be installed with minimal installation on your bathroom wall.
(Show me examples!)
Floor Standing -
A floor standing towel warmer can be installed to stand on the bathroom floor giving easy access to your towels.
(Show me examples!)
Shelf -
A shelf towel warmer can be installed in your bathroom on the wall. It conserves on space while adding a great look to your bathroom.
(Show me examples!)
Portable -
A portable towel warmer gives the convenience of easy installation anywhere in your home. Just plug in the towel warmer and receive warm towels.
(Show me examples!)
How to use towel warmers
When using towel warmers, towels should be folded to double thickness. This helps trap the heat in the fiber of the towel. You can put more than one towel at a time. In fact, the more towels you put on it the better it works! For quickest drying results the towel should be unfolded to allow the moisture to escape quickly.
When drying items and garments it is important that a towel is placed over the rail and the garments are placed on top of the towel. You need to be sure that items are colorfast to avoid discoloration or bleeding of color. Garments should be free of detergents or other residues that may cause discoloration. (Fabrics that contain soap or detergent residue may show what appears to be scorch marks. However, this is simply the discoloration of the residue. The heated towel rack does not reach sufficient temperature to scorch fabric).
For Phone Sales please call 1-516-749-6375.
We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
We carry all products from the brands you see on our website plus we also carry more brands not listed online. For
sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open
from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or,
contact us via email!