MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
There are many different aspects to consider when tackling the job of lighting the inside of your home. The following features will help you in making your lighting decision. Don't forget to keep this article for reference using our convenient printer-friendly version!

  • Lighting tips by room
  • Lighting tips by function
  • Light levels
  • Bulbs


    Lighting by Room
    Dining room
    Achieve overall illumination using chandeliers or pendants with 200-400 wattage. Install them 30” above the table to allow for head room when standing. The diameter of fixture should be 12” less than width of table. Then add matching wall mounts or recessed downlights to add accent sparkle. Don’t forget to light up the shelves of a hutch or cabinet!
    Kitchen
    From a functional standpoint, kitchens need both ambient (overall) and task lighting. For more detailed information, see "how to choose kitchen lighting."
    Bath, spa & vanity
    Considering bathrooms are used for so many functions, it is no wonder many considerations need to be addressed. For more detailed information, see "how to choose bathroom lighting."
    Entrance foyer / hallway
    Use a ceiling mount or pendant for general lighting to welcome guest in the foyer. For safety in hallways use lighting fixtures every 8 to 10 feet. These can be wall sconces, surface mounted or recessed ceiling fixtures. Chandeliers should hang approximately 30 inches above your tabletop and be 6 inches narrower than your table on each side. Choose a chandelier that fits the proportions of your dining room.

     Back to top or find indoor lighting now

    Lighting by Function
    Reading Light for reading should be equal to 100 w to 150 w incandescent and come from behind the reader’s shoulder to reduce shadows. Bottom edge of the shade should be at eye level when seated or approximately 40” to 42” above the floor. For reading in bed use two matching wall mounted or pendant fixtures installed 30” above the top of the mattress. For reading, place lamp alongside your shoulder, with the bottom of the shade even with your head. Extra tall lamps should be moved back 2 feet if possible.
    Task Lighting Designed to help you perform specific tasks such as reading, sewing, typing, hobbies, or paperwork. Lamps are commonly used for task lighting, because they are portable and flexible. Many "task" lamps contain halogen bulbs, which provide intense, focused light without glare or shadows. For reading, place lamp alongside your shoulder, with the bottom of the shade even with your head. Extra tall lamps should be moved back 2 feet if possible. Desk lamps should focus light on the work surface and be adjustable. The light should be about 15 inches from your desktop.
    Accent Lighting Designed to add drama and focus attention within a room. By spot lighting items such as paintings, houseplants, furniture, sculptures, dark corners, fireplaces, etc., you can highlight your room's best features. Accent lighting is most effective when you focus three times as much light on your focal point as the general lighting around it. Track lights, recessed lighting, or wall sconces are often used to provide accent lighting. Portable lamps such as torchieres and small accent lamps can also be used to feature certain areas of your room. Use several lamps in a room to avoid shadows and dark areas. (One standard lamp will illuminate 4050 square feet.) You generally want to position the lamp 36 inches or less from the item to be lit.
    Ambient Lighting Provides a room with overall illumination. Ambient lighting serves the same function as sunlight, allowing you to see and walk about safely. Table and Floor lamps can be strategically placed throughout your home to provide great ambient lighting.
    Utility Lighting When you need a lot of light, such as outdoors or when doing work around the home. This lighting type is used mainly to "flood an area."

     Back to top or find indoor lighting now

    Light Levels
    Light bulbs emit billions of little light particles from their surface. The amount of light particles emitted is called Lumens. If you look on a light bulb or on its package you will see how many Lumens the bulb emits; the higher the Lumens the more color we see.

    Depending on what type of activity you would like to perform there is recommended lighting levels. Because light levels change with the distance from its source, and items like shades and covers cut light, one can measure the light level using a light meter (costing approx. $30) which will read the light in terms of footcandles (i.e. the light that a candle produces 1 foot away unobstructed). Use the table below as your guide.

    Recommended Footcandles
    Activity Footcandles
    Casual reading 2050
    Intensive reading or studying 50100
    Kitchen & laundry 2050
    Dining & entertaining 1020
    Workshop 50100
    Model-building hobbies that require high detail 100200

     Back to top or find indoor lighting now

    Bulbs
    Once you’ve chosen the right lamp, you should consider the best bulb to get the job done. The most commonly used bulb types are:

    Incandescent
    Incandescent bulbs are the most commonly used in lamps because they are inexpensive and widely available. Most incandescent bulbs vary from 15 to 150 watts and produce a soft yellow-white light, emitted in all directions. They are generally available in clear, frosted, or colored. Incandescent bulbs are great for standard ambient lighting. Those with higher wattages are good for task lighting. (Remember: Never exceed the maximum wattage recommended for your lamp!)
    Halogen
    Halogen bulbs produce a bright, white light. They most closely replicate the color spectrum of the sun. Halogen bulbs have a longer life and provide more light (lumens) per watt than regular incandescent bulbs. Their small size and intensity make halogens great for task lighting. Note: Since halogen bulbs burn hotter than other types, they require more caution. All halogen lamps sold today in the USA have approved safety shields to reduce fire risk. When changing a halogen bulb, be sure to wait until the bulb cools to touch it. Always use a clean rag to handle a halogen bulb, as oils from your hand will cause the bulb to burn hotter and can greatly reduce the life of your bulb.
    Fluorescent
    Fluorescent bulbs are very energy efficient and use much less electricity than standard incandescent bulbs. They also can last up to 20 times longer! Their new compact styles make fluorescent bulbs practical for task lighting. Screw-in types can be used in place of incandescent bulbs in standard lamp sockets.

     Back to top or find indoor lighting now




    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan