MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
From a functional standpoint, kitchens need both ambient (overall) and task lighting. The following features will help you in making your lighting decision.

Good kitchen lighting, from an aesthetic and functional standpoint, incorporates both ambient and task lighting. This method of layering the light is important for achieving positive results in all types of living and working spaces.

Start with the task areas. These are best lit with bright, shadowless light. Fluorescent tubes are particularly well suited for this because of their large surface area and high lumens per watt (recommendation: T8 fluorescent lamps with electronic ballasts). You want to get the fixture close to the task area, (in kitchens this would be counters, sinks, and tables), so mounting the lights on the underside of the upper cabinets is convenient. In the case of an island or peninsula counter tops, with no upper cabinets to attach lights to, you need to use hanging pendant style fixtures or project light from the ceiling. If ceiling mounts are used then your choice will probably be incandescent lamps (either in track or recessed fixtures).

Think about ambient lighting. Ambient light is the general, overall light that fills in shadows, reduces contrast, and lights vertical surfaces to give the space a brighter feel. Ambient light is what you need for casual activities in your rooms. If the kitchen has light colored surfaces and lots of windows you should have plenty of natural ambient light during the day. But kitchens are used from before dawn until after midnight -- we can't rely on windows and skylights. Fluorescent tubes are well suited to the job of providing ambient light. They provide broad, even illumination and their efficiency makes it possible to fill the space with light without turning it into an oven.

Choose a color temperature of 3000K or 3500K for a warmer, more inviting appearance. You can put the tubes in a central fixture but you may want to try some other strategies, like placing them on top of the upper cabinets to indirectly reflect off a light colored ceiling. If you have at least 12 inches of space from the top of the upper cabinets to the ceiling, this is an inexpensive way to brighten up a kitchen. Or, maybe you have a custom pot rack hanging over an island and can build lighting into it to reflect off the ceiling and down onto the island.

Add a layer of accent lighting. Accent lighting is what gives our space a third dimension, adding to the quality of the space. Accent lighting is used sparingly on those special home objects that we want people to notice and admire. Accent lighting is usually done with spot lights. You may be lighting artwork, architectural details, collectibles, or a food presentation area.




For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
Kitchen Faucets
Kitchen Sinks
Garbage Disposers
Hot Water Dispensers
Pot Fillers
Faucets
Sinks
Tub Fillers
Showers
Jetted Tubs
Non-Jetted Tubs
Toilets & Bidets
Toilet Seats
Accessories
Ceiling Fans
Ceiling Lights
Chandeliers
Pendants
Sconces
Spot Lights
Vanity Lights
Desk Lamps
Floor Lamps
Table Lamps
Wall Lamps
Torchiere
Armoires
Cabinets
Mirrors
Shelves
Tables
Windows of Art
Clocks
Medicine Cabinets
Colanders
Pot Racks
Towel Warmers
MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan