MY SUPPLYHOUSE
 MY BASKET   Shopping Cart
0 Item(s) : $0.00
Check Out
Register Login

   -   HOME 
What’s your idea of the ideal shower… a fine tingly spray… a soft, drenching flow… a relaxing, pulsating massage? Or does it depend on your mood? Imagine having every option right at your fingertips! Transform your fantasy into a reality. Here’s what you’ll need to consider…

  • Showering space
  • Showerheads
  • Showerhead positioning
  • Bodysprays
  • Bodyspray positioning
  • Control valves: pressure balanced vs thermostatic
  • Who will be using the shower?
  • Installation
  • Choose from a variety of shower systems
  • Shower Accessories


    Showering space
    The minimum space required for a single person shower is 32” by 32”. When planning your shower, include adequate space for all users to comfortably maneuver but still be in close proximity to the shower and body sprays.

     Back to top or find a shower system now

    Choosing showerheads  (Show me examples!)
    You have many options when it comes to your showerhead…choose one or any combination of them all!
  • Fixed showerhead - Installed about 78” from the floor, an overhead shower is traditionally angled to spray out at shoulder height.
  • Handshower - Allows you the convenience of removing the showerhead to thoroughly rinse your hair, bathe young children, rinse down shower walls and more.
  • Handshower on a slide bar - Gives you all the convenience of a handheld shower plus it easily adjusts to each user’s different heights.
  • Overhead shower - Mounted on the ceiling, these overhead showers give you a “waterfall” feeling.

    Most showerheads and handshowers offer a variety of sprays. Some include conventional, aerated, needle, massage, soft or champagne flows.   (Show me examples!)

    Showerhead positioning
    Shower arms are usually installed at a 78” height, which locates the showerhead above the head of even the tallest user. Installing a handshower on a slide bar is ideal for a family because it easily adjusts to users’ different heights.

     Back to top or find a shower system now

    Choosing bodysprays  (Show me example!)
    Bodysprays and side sprays can be added to an overhead spray for whole body drenching. They can be added singularly or in pairs (up to the volume capacity of the shower control valve). Like showerheads, different bodysprays offer different spray options (see examples above). Don’t forget to add an On/Off Valve to have the option to turn the bodysprays off.

    The Kohler BodySpa is a shower system that is relaxing and beneficial. The BodySpa system operates similarly to a whirlpool, but in a vertical arrangement. Water is propelled through the air by bodyjets to maximize the effect of a hydro-massage. The BodySpa can double as a traditional showering space with the addition of a separate shower faucet and valve. So, you receive the experience of a shower and a whirlpool in one.

    Bodyspray positioning  (Show me a diagram!)
    Consider the height of the users. Concentration of sprays should be up to the shoulders (not to the face), the lower back and the knees/thighs. Spray jets can be installed to allow some “overlap” of sprays… the more water, the better! Each bank of two or three spray jets can be operated with their own volume controls. The highest spray jet should be operated separately for the tallest person using the shower, so the upper spray can be turned off not to hit shorter bathers in the face.

    Control valves: pressure balanced vs thermostatic
    The control valve is the driving force behind the shower system. It turns water on and off, adjusts water volume, controls temperature and directs water to showerheads and body/side sprays! There are two options, a pressure balancing or a thermostatic valve. Pressure balancing faucets automatically adjust the mix of hot and cold water to maintain a comfortable temperature even if water pressures changes (example: toilet flush). Thermostatic shower faucets take safety a step further. They adjust the hot and cold mix in response to pressure and/or temperature changes in the hot and cold water supplies... they will actually stay within 3 degree of the temperature you selected! As you can image, this gives you added control of your shower, and allows you to have an enjoyable and relaxing shower!

     Back to top or find a shower system now

    Who will be using the shower?
    You may want to consider separate control valves if more than one person will be showering at a time. Always remember that scald-protection safety valves are important for everyone, but especially children and the elderly.

    Installation
    Before you decide which shower installation you desire, it is important to review some of the basics of ultimate performance of your system with your plumber or licensed contractor:
  • Water pressure in your home
  • Water supply line size and the condition of the pipes
  • Water heater requirements
  • Drain pipe size and capacity
  • Convenience and safety
  • Local plumbing codes

     Back to top or find a shower system now

    Shower accessories   (Show me examples!)
    To compliment your shower system, don’t forget there are many shower accessories that will enhance the beauty and style of your shower. Choose from the following:
  • Shower baskets
  • Shower drains
  • Shower rods
  • Curtain rings
  • Grab bars
  • Soap dishes

    Choose from a variety of shower systems by:
  • Alsons
  • Grohe
  • American Standard

     Back to top or find a shower system now
    fixed showerhead
    handshower
    handshower on a slidebar
    overhead shower
    conventional
    aerated
    massage
    needle spray
    soft flow
    champagne flow
    spray patterns
    soap dish
    shower rod
    Kohler bodyspa



    For Phone Sales please call 1-516-749-6375. We specialize in decorative plumbing and lighting. Our top plumbing brands are Kohler, Blanco, Danze, Elkay, Franke, Kindred, and Moen. We have a warehouse full of these & other brands. Our top Lighting brands are PLC, Quoizel, & Thomas. For item availability, stock status or lead times, please email us or call 1-516-749-6375. Or else, place your order online, and we will alert you of any lead time.
    Kitchen Faucets
    Kitchen Sinks
    Garbage Disposers
    Hot Water Dispensers
    Pot Fillers
    Faucets
    Sinks
    Tub Fillers
    Showers
    Jetted Tubs
    Non-Jetted Tubs
    Toilets & Bidets
    Toilet Seats
    Accessories
    Ceiling Fans
    Ceiling Lights
    Chandeliers
    Pendants
    Sconces
    Spot Lights
    Vanity Lights
    Desk Lamps
    Floor Lamps
    Table Lamps
    Wall Lamps
    Torchiere
    Armoires
    Cabinets
    Mirrors
    Shelves
    Tables
    Windows of Art
    Clocks
    Medicine Cabinets
    Colanders
    Pot Racks
    Towel Warmers
    MFG List: AF Lighting | Afina | Alsons | American Standard | AquaPure | Aupu | Bates and Bates | Bemis | Besa | Blanco | Brondell | California Faucets | Chicago Faucets | Church | Cole & Co | CSI Donner | Cucina | Danze | DDS | Decolav | Delta | Designers Fountain | Dyson | Elizabethan Classics | Eljer | ELK Lighting | Elkay | Franke | Garvin | Ginger | Grohe | Hamat | Hansgrohe | Herbeau | Hunter | InSinkErator | Irritrol | Jacuzzi | Jado | Kenroy Lighting | Kichler | Kindred | Kingston Brass | Kohler | KWC | Legend | Linea Aqua | Mico | Moen | Monte Carlo | MrSauna | MrSteam | Myson | Newport Brass | NuTone | Olsonite | Panasonic | PLC Lighting | Porcher | Price Pfister | Quoizel | Rain Bird | Renova | Rialto | Robern | Rohl | Saniflo | Sea Gull | Showhouse | Smedbo | Soehnle | Speakman | St Thomas Creations | Sunrise Specialty Co | Swanstone | Thermasol | Thomas Lighting | Toro | Toto | Tread Safe | Trend Lighting | Triarch International | Victoria & Albert | Vita Bath | Volume | Vostra | WarmaTowel | Warmrails | Wasauna | World Imports

    We carry all products from the brands you see on our website plus we also carry more brands not listed online. For sales assistance, please call one of our friendly Sales Representatives Toll-Free at 1-516-749-6375. We are open from 8AM to 7PM EST Monday to Friday and from 10:30AM to 4:30PM Saturdays. Or, contact us via email!

    Internet Security By ControlScan   Internet Security By ControlScan   Internet Security By ControlScan