PEX-AL-PEX

 
 

Rifeng PEX-AL-PEX Tubing

This category contains PEX-Aluminum-PEX (PEX-AL-PEX) tubing manufactured by Rifeng.

FostaPEX PEX-AL-PEX Tubing

FostaPEX tubing adds aluminum and PE outer layers to the tubing to provide form stabi

Uponor Multi-Layer Composite (MLC) PEX-AL-PEX Tubing

Uponor Multi-layer Componsite (MLC) (formerly MultiCor) is a multi-layered composite

PEX-al-PEX Tools

Includes chamfering tools and the Fostapex prep tool. The chamfering tools prepare Mu

 

About PEX-AL-PEX

PEX-AL-PEX, also called Aluminum PEX, is a 3-layer oxygen barrier PEX tubing. This tubing has an aluminum core that holds its shape when bent so you don't have to tie it down every few feet like traditional PEX tubing. PEX-AL-PEX has the same temperature/pressure ratings as regular PEX, however it is better suited for high temperature applications, such as baseboard and fan coils because the aluminum core allows the tubing to maintain its shape. PEX-AL-PEX also has a lower linear expansion rate, which means that it expands less than regular PEX or copper as it heats up.