Apply to be a TradeMaster!
Main product image of Poly Tape (Indoor/Outdoor Use)
Magnifying glass
Hover image to zoom

Poly Tape (Indoor/Outdoor Use)

Brand:
K-Flex
SKU:
POLYTAPE
Rating:
(6)
Q&A:
(3)
Poly Tape (Indoor/Outdoor Use)
Magnifying glass
Hover image to zoom
POLYTAPE has been discontinued
Discontinued September 19, 2023
This product was discontinued by the manufacturer.
Suggested Alternative:
Line Set Tape - Black (1.88" x 180')
SKU:1507-B
(4)
Order by 6PM, receive 65 by Tomorrow
VIEW ALTERNATIVE
VIEW ALTERNATIVE

Product Highlights

–
Product Highlight: Color
Black

Description

–
Poly Tape is a convenient and easy to use product which complements the Nomaco Insulation tubing and sheet insulation products. It is supplied in 3 mil thickness by 2" width by 36 yards, with a solvent acrylic adhesive for applying to hot or cold pipe fittings.

Poly Tape is designed to perform in direct sunlight and is 25/50 rated for flame spread and smoke developed. It is waterproof and designed for indoor or outdoor use. Its function is to cover circumferential/butt joints, copper couplings and press fittings to ensure the seams from popping open.

Specs

–
Application:

Accessory

Color:

Black

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


Product Reviews

5 out of 6 reviews
100% would recommend this product
5
out of 6 Reviews
100% would recommend this product
WRITE A REVIEW
5 star
100%
4 star
0%
3 star
0%
2 star
0%
1 star
0%
WRITE A REVIEW
Showing 1-6 of 6 reviews

Just what I needed and works great

works good
Day Tripper
ok
11 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Better than duct tape

This is really interesting tape. Thin and non-stretchy but the adhesive sticks to just about anything that isn't wet. I use this to secure foam pipe insulation but have started to use it for taping seams in sheet goods and vapor barrier.
elf55
Virginia
11 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works great

I used this on the pipe that goes from my air conditioning unit into the house. It worked great to seal the ends before and after putting insulation on the pipe. Be sure to wipe the pipe dry before putting it on the pipe though or it will not stick otherwise it sticks to everything else great.
Dragon
North Liberty, IA
11 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

glad i had it

taped 10 lengths of 6'tube insulation together to feed thru 4" drain pipe with 3/4" poly pipe in a creek pipe bridge construction. Clerk said the tape was an overkill but I'm glad I had as it was strong and made a continuous tube out of the 10 pieces that were easier to feed thru the drain pipe. It was slick too and kept the joints from sticking into the inside of the pipe. Good stuff and a great $5 investment for a nice job
MT Man
Waynesville, NC
11 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Excellent tape

I wish I would have known about this tape years ago! It has excellent adhesion and is great for applying to pipe insulation, and many other assorted uses where a dark color waterproof tape is needed.
recycleman5
Philadelphia, PA
14 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

great tape to protect pipe insulation

you can use this tape on solar close loop systems to protect insulation from sun
p
Telford PA
15 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Product Q&A

3 Questions
3 Questions
ASK A QUESTION

Q: I plan to run a 50' 1/2" PEX line across my roof to a Solar Collector for Solar Hot Water. Could I use your foam pipe insulation and then cover it with Poly Tape to make it UV resistant?

Asked by Jan 14 years ago

Add your answer

* Required Field
-

I'm not sure about the tape, I'd guess the poly tape would start to come apart pretty quickly and then the crows would start picking at the foam. I believe the rubitex holds up better against the UV, but you'll want to check that. On another note. Pex and even Pex-Al-Pex aren't rated for the high water temperatures any sort of glazed solar collector is going to generate, flat plate or evacuated tube. It may work for awhile, but eventually you'll have the pex blow out right at the connections to the collector. Some people try to get away with a few feet of copper right at the connections, but I generally think it's a bad idea. When your collector flashes to steam for whatever reason that steam expands and takes up a lot of volume and will transfer all of that heat to the pex. You really should use copper or there is flexible stainless steel lines that are available. The flexible stainless steel is essentially natural gas flex pipe, but sometimes a bit different steel.

Was this review helpful to you?
-

I used the foam insulation for the straight runs of the A/C piping. The tape is used at the joints of the foam and at the irregular piping surfaces – valving. Taping the entire run after covering in foam was not done but probably would not hurt as long as one did not crush the foam insulation. The foam has built in adhesive at its mating edge.

Was this review helpful to you?

Q: Recently had a new unit compressor/condensor installed. After installation I noticed I could see the copper tubing underneath some old foam "pipe" at the connection point. I called the installer and asked that he address this condition using areosol foam. Will this foam do the same as using poly tape and/or your "pipe"? FYI-saw a pic/description of using your products for this reason- fixing rotting A/C insulation in Familyhandyman, 10/2010 issue while waiting in a dr's office. I thought I had lost it and just found it after the installation. Maybe we could have saved a little if I put the paper away in a convenient location. Thanks for your reply. Margaret

Asked by Margaret - Mrs. Fixitinmyhouse 15 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

The foam, the pipe insulation, and this Poly Tape will all so the same thing. The tape can be used outdoors in temperatures down to -35 °F. It is waterproof and UV resistant.

Was this review helpful to you?

Q: Can this tape be used to protect PEX exposed to sunlight? I want to use PEX for an irrigation system and will have small lengths exposed that attached to the valve system to sunlight. I read somewhere to be careful about the type of adhesive that one can attach to PEX, as some of it will eat at the PEX tubing.

Asked by Ken 16 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

This tape is not designed for direct contact with PEX. We would recommend that you sleeve the exposed PEX with PVC.

Was this review helpful to you?