Apply to be a TradeMaster!

PEX-AL-PEX

PEX-AL-PEX tubing is a multi-layer pipe with a layer of aluminum sandwiched between two layers of cross-linked polyethylene (PEX). It combines PEX's flexibility with aluminum's resistance to expansion and oxygen permeation. It's widely used in radiant floor heating, snow melt systems, and some potable water applications. Its ability to hold a bent shape without kinking or springing back simplifies installation.

The lineup here covers PEX-AL-PEX tubing along with the compression fittings and specialized tools needed to cut, bend, and connect it. PEX-AL-PEX behaves differently from standard PEX-A or PEX-B tubing during installation, particularly in how it holds a bend. It generally requires its own fitting and tool compatibility rather than mixing in standard PEX components.

Resources
FAQs, Manuals & Videos
Videos
Articles
More About PEX-AL-PEX

Subcategories

  • Bluefin PEX-AL-PEX Tubing: Bluefin PEX-AL-PEX tubing combines an aluminum core with inner and outer PEX layers. Unlike standard PEX-A or PEX-B tubing, it holds a bent shape without kinking or springing back. It's commonly used in radiant floor heating and snow melt systems where a tubing run needs to hold a specific bend pattern. Sizing and layout follow the same design principles as other radiant tubing, based on the heating load and loop length.
  • PEX Radiant Compression Fittings: PEX radiant compression fittings join PEX-AL-PEX tubing using a compression ring and nut tightened over the tubing end, a mechanical connection method suited to the tubing's layered construction. They're specific to PEX-AL-PEX and generally aren't interchangeable with fittings designed for standard PEX-A or PEX-B tubing. Correct torque on the compression nut is necessary for a reliable seal.
  • PEX-al-PEX Tools: The category covers the specialized tools used to cut, bend, and prepare PEX-AL-PEX tubing for installation, including tubing cutters and bending tools suited to the tubing's aluminum core. Standard PEX-A or PEX-B tools don't always work correctly with PEX-AL-PEX's layered construction, so tooling compatible with this tubing type is generally needed on the job. Using the correct bending tool helps avoid kinking the aluminum layer during installation.

Buying Guide

PEX-AL-PEX tubing is generally chosen over standard PEX-A or PEX-B for radiant heat and snow melt installations. These jobs need tubing that holds a specific bend radius without kinking or springing back to its original shape. Its aluminum core gives it that shape memory, which simplifies routing tight bends compared to standard PEX.

Compression fittings designed specifically for PEX-AL-PEX's layered construction are necessary for a reliable connection. Fittings designed for standard PEX-A or PEX-B tubing generally aren't compatible with the added aluminum layer. Confirming that fittings are rated for PEX-AL-PEX specifically, rather than PEX in general, avoids an improper connection.

Cutting and bending tools also need to match the tubing type. A standard PEX cutter can usually cut PEX-AL-PEX cleanly. Bending it without kinking the aluminum core typically calls for a bending tool designed for that purpose, rather than bending the tubing by hand.

Loop length and layout planning for radiant heat and snow melt systems follow similar principles across tubing types. They are based on the heating load, floor or slab area, and the manifold's available ports. PEX-AL-PEX's ability to hold a bend can simplify routing around obstacles compared to standard PEX, but total loop length limits still apply based on the system's design.

Oxygen permeation resistance is one of PEX-AL-PEX's advantages in closed-loop hydronic systems. Its aluminum layer blocks oxygen diffusion that can otherwise contribute to corrosion in ferrous system components like a boiler or circulator pump. That makes it a common choice in radiant heat systems, where minimizing oxygen ingress protects the rest of the hydronic system.

Frequently Asked Questions

What makes PEX-AL-PEX different from standard PEX tubing?

PEX-AL-PEX has an aluminum layer sandwiched between two PEX layers. This gives it the ability to hold a bent shape without kinking or springing back, along with resistance to oxygen permeation. Standard PEX-A and PEX-B tubing don't have that aluminum core and behave more flexibly during installation.

Can standard PEX fittings be used on PEX-AL-PEX tubing?

No. PEX-AL-PEX generally requires fittings and tools designed specifically for its layered construction. Fittings made for standard PEX-A or PEX-B tubing typically aren't compatible with the added aluminum layer and shouldn't be substituted.

Why is PEX-AL-PEX common in radiant floor heating?

Its ability to hold a bend without kinking makes routing tight turns in a radiant floor loop easier than with standard PEX tubing. Its aluminum core also blocks oxygen permeation, which helps protect ferrous components elsewhere in a closed-loop hydronic system from corrosion.

Does PEX-AL-PEX need special tools to bend correctly?

A bending tool designed for PEX-AL-PEX's aluminum core helps form a bend without kinking the tubing, which can happen more easily with this tubing type than with standard PEX. Hand-bending without the correct tool increases the risk of damaging the tubing.

Is PEX-AL-PEX suitable for potable water applications?

Some PEX-AL-PEX products are rated for potable water use. It's more commonly specified for radiant heat and snow melt systems, where bend retention and oxygen barrier properties are the main advantages. Checking the specific product's rating and local plumbing code before use is necessary for a potable water application.

Resources

Videos
Watch the product video for undefinedPlay Icon
How To Use A PEX-AL-PEX Chamfering Tool
More About PEX-AL-PEX

Subcategories

  • Bluefin PEX-AL-PEX Tubing: Bluefin PEX-AL-PEX tubing combines an aluminum core with inner and outer PEX layers. Unlike standard PEX-A or PEX-B tubing, it holds a bent shape without kinking or springing back. It's commonly used in radiant floor heating and snow melt systems where a tubing run needs to hold a specific bend pattern. Sizing and layout follow the same design principles as other radiant tubing, based on the heating load and loop length.
  • PEX Radiant Compression Fittings: PEX radiant compression fittings join PEX-AL-PEX tubing using a compression ring and nut tightened over the tubing end, a mechanical connection method suited to the tubing's layered construction. They're specific to PEX-AL-PEX and generally aren't interchangeable with fittings designed for standard PEX-A or PEX-B tubing. Correct torque on the compression nut is necessary for a reliable seal.
  • PEX-al-PEX Tools: The category covers the specialized tools used to cut, bend, and prepare PEX-AL-PEX tubing for installation, including tubing cutters and bending tools suited to the tubing's aluminum core. Standard PEX-A or PEX-B tools don't always work correctly with PEX-AL-PEX's layered construction, so tooling compatible with this tubing type is generally needed on the job. Using the correct bending tool helps avoid kinking the aluminum layer during installation.

Buying Guide

PEX-AL-PEX tubing is generally chosen over standard PEX-A or PEX-B for radiant heat and snow melt installations. These jobs need tubing that holds a specific bend radius without kinking or springing back to its original shape. Its aluminum core gives it that shape memory, which simplifies routing tight bends compared to standard PEX.

Compression fittings designed specifically for PEX-AL-PEX's layered construction are necessary for a reliable connection. Fittings designed for standard PEX-A or PEX-B tubing generally aren't compatible with the added aluminum layer. Confirming that fittings are rated for PEX-AL-PEX specifically, rather than PEX in general, avoids an improper connection.

Cutting and bending tools also need to match the tubing type. A standard PEX cutter can usually cut PEX-AL-PEX cleanly. Bending it without kinking the aluminum core typically calls for a bending tool designed for that purpose, rather than bending the tubing by hand.

Loop length and layout planning for radiant heat and snow melt systems follow similar principles across tubing types. They are based on the heating load, floor or slab area, and the manifold's available ports. PEX-AL-PEX's ability to hold a bend can simplify routing around obstacles compared to standard PEX, but total loop length limits still apply based on the system's design.

Oxygen permeation resistance is one of PEX-AL-PEX's advantages in closed-loop hydronic systems. Its aluminum layer blocks oxygen diffusion that can otherwise contribute to corrosion in ferrous system components like a boiler or circulator pump. That makes it a common choice in radiant heat systems, where minimizing oxygen ingress protects the rest of the hydronic system.

Frequently Asked Questions

What makes PEX-AL-PEX different from standard PEX tubing?

PEX-AL-PEX has an aluminum layer sandwiched between two PEX layers. This gives it the ability to hold a bent shape without kinking or springing back, along with resistance to oxygen permeation. Standard PEX-A and PEX-B tubing don't have that aluminum core and behave more flexibly during installation.

Can standard PEX fittings be used on PEX-AL-PEX tubing?

No. PEX-AL-PEX generally requires fittings and tools designed specifically for its layered construction. Fittings made for standard PEX-A or PEX-B tubing typically aren't compatible with the added aluminum layer and shouldn't be substituted.

Why is PEX-AL-PEX common in radiant floor heating?

Its ability to hold a bend without kinking makes routing tight turns in a radiant floor loop easier than with standard PEX tubing. Its aluminum core also blocks oxygen permeation, which helps protect ferrous components elsewhere in a closed-loop hydronic system from corrosion.

Does PEX-AL-PEX need special tools to bend correctly?

A bending tool designed for PEX-AL-PEX's aluminum core helps form a bend without kinking the tubing, which can happen more easily with this tubing type than with standard PEX. Hand-bending without the correct tool increases the risk of damaging the tubing.

Is PEX-AL-PEX suitable for potable water applications?

Some PEX-AL-PEX products are rated for potable water use. It's more commonly specified for radiant heat and snow melt systems, where bend retention and oxygen barrier properties are the main advantages. Checking the specific product's rating and local plumbing code before use is necessary for a potable water application.