Shop Resideo Sale
Main product image of PEX Crimp Starter Kit
Magnifying glass
Hover image to zoom

PEX Crimp Starter Kit

Brand:
Bluefin
SKU:
CRIMPPACK
Rating:
(8)
Q&A:
(7)
PEX Crimp Starter Kit
Magnifying glass
Hover image to zoom
$508.43 each
In Stock
In Stock
Get 32 Tue, Nov 17
Order by today, receive Tuesday
Free Shipping This item ships free
Easy Returns No restocking fee for 90 days

Product Highlights

–
Product Highlight: Fitting System Compatibility
Crimp, Clamp
Product Highlight: Tubing Compatibility
PEX
Product Highlight: Tubing Type
Non-Oxygen Barrier
Product Highlight: Length
200 ft. (3/4"), 200 ft. (1/2")

Description

–

The PEX Crimp starter kit is great for a DIY or professional looking to get started with PEX Plumbing or the PEX Crimp System specifically.

This kit contains the following products:

  • PXTLKIT-2 (1): The kit, with a tough plastic case, includes a 15" Master Crimper that crimps 3/8", 1/2", 5/8", 3/4", and 1" copper crimp rings, interchangeable 3/8", 1/2", 5/8", 3/4", and 1" crimping jaws, and a Go/No-Go crimp gauge. Crimp tool conforms to ASTM F1807 specifications for PEX connections in potable water and radiant heating systems.
  • PXCR050 - 1/2" PEX Crimp Rings (100): Copper Crimp Rings For PEX Connections.
  • PXCR075 - 3/4" PEX Crimp Rings (50): See EPCR0012 (above) for description.
  • PXE050-DZR - 1/2" PEX x 1/2" PEX Brass Elbows (25): May be used with the stainless steel clamping system or the copper crimp ring system.
  • PXE075-DZR - 3/4" PEX x 3/4" PEX Brass Elbows (25): See H000500LF (above) for description.
  • PXC050-DZR - 1/2" PEX x 1/2" PEX Brass Couplings (25): Makes PEX to PEX connections for PEX Tubing. May be used with the stainless steel clamping system or the copper crimp ring system.
  • PXC075-DZR - 3/4" PEX x 3/4" PEX Brass Couplings (25): See PXC050 (above) for description.
  • TU050-100-B - 1/2" Blue Bluefin Tubing 100 ft. coil (1): Bluefin PEX pipe is produced with crosslinked polyethylene. Crosslinking is obtained through a chemical process that increases the bonds between macromolecules to form a more complex structure than the normal polyethylene.
  • TU050-100-R - 1/2" Red Bluefin Tubing 100 ft. coil (1): See TU050-100-B (above) for description.
  • TU075-100-B - 3/4" Blue Bluefin Tubing 100 ft. coil (1): See TU050-100-B (above) for description.
  • TU075-100-R - 3/4" Red Bluefin Tubing 100 ft. coil (1): See TU050-100-B (above) for description.
  • E6081128 - Tube Cutter, (plastic) up to 1" PEX

Specs

–
Type:

Crimp

Fitting System Compatibility:

Crimp

Clamp

Tubing Compatibility:

PEX

PEX Size:

3/4"

1/2"

Tubing Type:

Non-Oxygen Barrier

Length:

200 ft. (3/4")

200 ft. (1/2")

Contact

Help Face
CALL US
Question? Call or text 888-757-4774
+
Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


Product Reviews

4.5 out of 8 reviews
86% would recommend this product
4.5
out of 8 Reviews
86% would recommend this product
WRITE A REVIEW
5 star
75%
4 star
13%
3 star
0%
2 star
13%
1 star
0%
WRITE A REVIEW
Showing 1-8 of 8 reviews

30 years experience

I'm a plumber with 30 years experience in commercial and residential Plumbing. I have dealt with copper CPVC PEX uponor and galvanized and dealing with each one of these PEX and uponor are in my opinion the two easiest to deal with no matter if they come on rolls or not. Copper in itself is disgusting when you take it out of a home oxidized with green on the inside because everyone knows water and metal don't mix unless you're dealing with stainless steel or brass. CPVC should be outlawed because it becomes brittle overtime and will split and break like glass. It is a very dangerous water pipe about like polybutylene. This is my experience with PEX I have yet to be called back because of a crimp ring or bad fitting now I am meticulous and very OCD with everything I do. I would definitely recommend this product to anyone but please seek out a professional to install this product and show you how it works. PEX and uponor which is a form of PEX is 100% the way to go. No glue no solder joints which is better for you and your body. Have a great day everyone
Tony the plumber
Canton GA
8 years ago
Was this review helpful to you?

Not what I expected

This being my first PEX job but with 30 years of construction experience. I have built 2 houses completely by myself for myself. These rolls come and the shape is left to fight. You can't even get a accurate measurement when every pipe keeps the roll shape. I have 3 ft drill bits to get me through anything. You can't get curved pipe through straight drilled holes. what this kit cost plus all other fitting I need. The only parts of PEX I didn't fight was the scrap pieces. If you need 6 ft to do a 4 ft section cuz you can't get the bend out, what is the point. For the experienced do it yourselfers do your homework. I thought I did. If the point is that PEX won't freeze and break. Cpvc has never failed me or copper. Insulated pipes don't freeze. What good is a frozen water line that won't break if I can't get water ?
Grumpy
Elma Washington
9 years ago
Was this review helpful to you?

Good Stuff!

I replumbed my house with pex using this kit. My water pressure is better. My lines are more managable and I took out $500 in copper. What's more... no leeks. I am happy.
Hugh
Ogden, Utah
13 years ago
Was this review helpful to you?

Fantastic!!!

This was the easiest product I have used in a very long time. I was skeptical if the connections would hold under the water pressure. Everything worked perfect. I used the starter kit for our summer vacation home. Most of the new water lines are outside. After replacing all the cracked lines, we probably saved hundreds of dollars we would have normally spent on a plumber(time is money). We were done quickly and no messy cleanup. We have more than enough for many more repair projects in the future. I highly recommend this product.
Bungalow Boys
New York
15 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Good product to get started with PEX

This was my first experience with PEX and the kit supplied everything I needed. When combined with the manabloc manifold, this system makes plumbing a breeze for the DIYer.
happy
Sallisaw
16 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

good stuf

i was using this to run plumbing too a 9000 sf home remove all the old m copper and pex look great great pressure. and the best part it will not break this winter:D
RoVERT
binghamanton ny
16 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Great Starter Kit

I moved into a House that was built completely using PEX, Being use to PVC I realized if something leaked I wouldn't be able to fix it. After researching PEX I found PEX Supply and this kit, This Kit gives you everything you need to handle most PEX jobs minus valves, tees etc.. But what you get is a well thought out kit. The Crimping Tool is a Pretty Good tool that allows tension adjustment and easily change out of jaws. I just used this to install a Water Softener and Whole House water Filter, The Install went Flawless and the only leaks I had, weren't with the PEX but instead with the cheap plastic fittings that came with the softener/filter. Never using PEX before in my life, I was surprised at having no leaks on the PEX. I'd highly recommend this kit for any homeowner with a PEX home and a Great starter kit to the beginning PEX plumber. TJB
TJB
Orange, VA
16 years ago
Was this review helpful to you?

Very Complete Kit

Great starter kit with enough of what you need to see how the system works. The support video on the Pex website explains how to use everything.
Jeff
Newtown, CT
16 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Product Q&A

7 Questions
7 Questions
ASK A QUESTION

Q: What type of pex (A, B, C) is this?

Asked by Ash 10 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse Staff

The pex tubing in this kit is pex B.

Was this review helpful to you?

Q: Can i use this starter kit with potable water. thanks Emile

Asked by emile 11 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- Supplyhouse Staff

yes it is

Was this review helpful to you?

Q: What is the difference between the pex Crimp and the pex clamp systems?

Asked by k 14 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

Please refer to the link below. http://pexsupply.blogspot.com/2011/08/pex-crimp-vs-pex-clamp-fittings.html

Was this review helpful to you?
-

none

Was this review helpful to you?

Q: When and why would we use the crimping tool?

Asked by Tom 15 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

There are several varieties of PEX fittings. These include crimp, clamp, press, expansion, compression, and push-fit. You would use the crimping tool if you need to make a PEX fitting connection and you opt to use the crimp method.

Was this review helpful to you?

Q: 1)What is the purpose of the gauge tool? Is it to measure the roundness of the pex prior to crimping? 2) You mentioned barrier oxygen px for heating system to prevent rusting in the system. Rusting in what system? On the medal basboard itself?

Asked by 15 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

A go-no-go gauge is used on crimp rings after a fitting has been made. If a ring does not fit into the gauge at all, or goes all the way through to the bottom, the fitting was made incorrectly. This is demonstrated in our PEX crimping video ( http://www.youtube.com/watch?v=KnZorlmOOf8 ). The rusting you mention would occur on any ferrous metal that the water touches throughout the heating system. The outer baseboard covers and inner copper elements would be unaffected. It is mainly an issue for cast iron circulator pumps and boilers.

Was this review helpful to you?
- Mr know all

The gauge tool measures the outside diameter of the finish crimped connection. Too big? Crimp more so it grips the pex tubing. 2) oxygen getting inside the lines will corrode the inside of and cast iron or galvanized pipe or circulation pumps which are typically cast iron housing. The metal in most hydronic baseboards are copper with aluminum heat sink fins.. Of which neither oxygen effects much at all, or takes very long time. Mind you, this is happening on the inside of the components.

Was this review helpful to you?

Q: can i use the included 3/4 tubing in the package with baseboard heating....otherwise,is it oxygen barrier tubing?

Asked by hunter 15 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

You can use 3/4" PEX in a baseboard system, but you should use PEX with an oxygen barrier to prevent rusting in the system. This package includes non-oxygen barrier tubing.

Was this review helpful to you?

Q: will pex withstand freezing while in use

Asked by 15 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- PexSupply Staff

PEX, since it is able to expand, is more freeze-resistant than copper. Still, PEX is not freeze-proof. It can burst if water freezes.

Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy