ClimateMaster designs and manufactures water-source and geothermal heat pump systems. These serve residential and commercial buildings. The company was founded in Florida in the late 1950s and later relocated to New York. It eventually settled in Oklahoma City. Its Oklahoma City plant spans 510,000 square feet and supports over 600 American jobs along with a network of more than 1,200 independent dealers.
ClimateMaster operates as a subsidiary of Climate Control Group, which is owned by NIBE, a manufacturer focused on sustainable heating technology. Its geothermal systems draw on the stable temperature of the earth to heat and cool buildings. This differs fundamentally from air-source equipment, which has to work against outdoor temperature swings.
Product Lines
SupplyHouse carries ClimateMaster's water-source and geothermal heat pump lineup. It includes equipment for vertical and horizontal closed-loop installations, as well as open-loop systems for sites with a suitable water source. The range spans residential split and packaged units alongside light commercial equipment sized for schools, offices, and multifamily buildings.
ClimateMaster also manufactures water-to-water heat pumps for radiant floor heating and domestic hot water applications. These give contractors options beyond standard forced-air geothermal setups when a project calls for hydronic distribution.
Why Contractors Specify ClimateMaster
Contractors often turn to ClimateMaster because its equipment is engineered and assembled in the United States, which simplifies warranty support and parts sourcing compared with some imported alternatives. Geothermal systems draw heat from the ground rather than outside air. Performance holds steady through extreme winter cold and summer heat, conditions where air-source heat pumps typically lose capacity.
The company has produced water-source equipment for decades. Contractors bidding geothermal retrofits and new construction projects can find a wide range of capacities and configurations from a single manufacturer. This cuts down on the number of vendors needed for one job.
How to Choose ClimateMaster Products
Selecting a ClimateMaster system starts with the loop type available on site. Closed-loop vertical systems work well on smaller lots where horizontal trenching isn't practical, while horizontal loops suit properties with more available land and lower installation cost. Open-loop systems make sense only where a suitable water source, such as a well, meets local code and water-quality requirements.
Contractors should also match unit capacity to the building's heating and cooling load rather than oversizing, since geothermal equipment runs most efficiently near its rated capacity. For radiant heating or domestic hot water projects, a water-to-water unit is the right fit instead of the standard water-to-air package.
Frequently Asked Questions
What is the difference between open-loop and closed-loop ClimateMaster systems?
Closed-loop systems circulate a sealed fluid loop through vertical boreholes or horizontal trenches and return it to the heat pump without contacting groundwater. Open-loop systems draw water directly from a well or similar source, use it for heat exchange, then discharge it, which requires adequate water volume and quality at the site.
Can ClimateMaster equipment connect to existing ductwork?
Many ClimateMaster water-to-air units are sized to work with existing residential duct systems, though a load calculation should confirm the ductwork can handle the new unit's airflow requirements. Water-to-water units bypass ductwork entirely since they serve radiant floor loops or other hydronic distribution.
Does ClimateMaster make equipment for commercial buildings?
Yes. ClimateMaster manufactures light commercial water-source heat pumps sized for schools, offices, multifamily housing, and similar buildings, in addition to its residential product line.
Where is ClimateMaster equipment manufactured?
ClimateMaster equipment is engineered and assembled at the company's plant in Oklahoma City, Oklahoma, a facility that spans 510,000 square feet.
Who owns ClimateMaster?
ClimateMaster is a subsidiary of Climate Control Group, which is in turn owned by NIBE, a manufacturer focused on sustainable heating technology.