Cross Manifold is a hydronic manifold system manufactured by Ultra-Fin Inc. The product line is built around a fully assembled zoning package. It ships as one unit with a stainless steel manifold body, ball valves, temperature gauges, bleed valves, fittings, an automated control, and a power supply.
Rather than requiring a contractor to source and assemble each zoning component separately, the system arrives ready to mount and wire into a radiant or radiator loop. Cross Manifold serves both new hydronic installs and retrofit projects where a compact, factory-built zoning package simplifies the mechanical room layout.
Product Lines
The core Cross Manifold product is available in five circuit configurations of 4, 6, 8, 10, and 12 zones. A contractor can size the manifold to the number of loops in a given system rather than combining smaller units.
Manifold bodies are constructed from 304 stainless steel for corrosion resistance in a wet mechanical room environment. Each unit pairs the manifold body with an automated valve control that opens and closes zone valves as called for by the system. The control draws power only during the brief moments a valve is actuating.
The line supports pure radiant heat loops, standard radiator loops, and combined radiant-and-radiator systems on the same manifold platform.
Why Contractors Specify Cross Manifold
Contractors working on multi-zone hydronic jobs often cite the factory-assembled format as the main draw. The manifold, valves, gauges, and control arrive matched and wired. This cuts field assembly time compared to building a zoning panel from individual parts.
The 304 stainless steel construction holds up in mechanical rooms where humidity and mineral buildup shorten the life of lower-grade materials. Because the valve control only draws power during a switching event rather than holding continuously, it adds little standby load to the system.
The same manifold platform covers radiant, radiator, and mixed systems. A contractor can standardize on one product family across different job types instead of stocking separate manifold lines.
How to Choose Cross Manifold Products
Selecting a Cross Manifold starts with counting the zones the job requires. Match that number to the closest available configuration among the 4, 6, 8, 10, and 12 circuit options rather than oversizing the unit.
Next, a contractor should confirm whether the loop is pure radiant, pure radiator, or a mix of both. The manifold platform is built to run either type from the same body.
Mechanical room space and mounting orientation also factor into layout, since the manifold, control, and power supply ship as a single assembly with a fixed footprint. Finally, verify the zone control's wiring matches the thermostats and staging equipment already specified for the job before finalizing the order.
Frequently Asked Questions
What is included in a Cross Manifold system?
A Cross Manifold ships as one assembly containing the stainless steel manifold body, ball valves, temperature gauges, bleed valves, fittings, an automated valve control, and a power supply.
What circuit configurations does Cross Manifold offer?
The manifold is available in five configurations: 4, 6, 8, 10, and 12 circuits. A contractor can match the unit to the number of zones on the job.
What material are the manifold bodies made from?
The manifold bodies are constructed from 304 stainless steel, which resists corrosion in humid mechanical room conditions.
Can Cross Manifold run both radiant heat and radiators?
Yes. The same manifold platform supports pure radiant loops, standard radiator loops, and systems that combine both on one manifold.
When does the valve control draw power?
The automated control draws power only while a valve is actively opening or closing, rather than holding power continuously between switching events.