Detroit Radiant Products Company was founded in 1955 and has spent over 70 years manufacturing energy-efficient heating equipment. The company operates from Warren, Michigan, running its own on-site testing laboratory and tooling operations rather than outsourcing production.
Detroit Radiant sells its heating equipment under the Re-Verber-Ray brand name, serving commercial, industrial, and agricultural markets that need infrared and forced-air heating solutions for large or difficult-to-heat spaces.
Product Lines
SupplyHouse carries Detroit Radiant's infrared tube heaters, along with patio heaters from the brand's Designer Series for outdoor comfort applications. The lineup also includes hot air unit heaters for general space heating and electric infrared heaters for locations where a gas line isn't practical.
Detroit Radiant additionally manufactures process burners for industrial heating applications. It also makes industrial LED lighting fixtures under its Lumerica line. This gives contractors a single source for combined heating and lighting projects in commercial buildings.
Why Contractors Specify Detroit Radiant
Contractors specify Detroit Radiant because the company has run its own manufacturing and testing operations in Warren, Michigan for decades rather than relying on third-party production. Building tube heaters, patio heaters, and process burners under one roof lets Detroit Radiant control tolerances and consistency across its product range.
Infrared heating from Detroit Radiant suits large open spaces such as warehouses, garages, or agricultural buildings. It reduces the ductwork typically required by forced-air systems. This simplifies installation in structures where running ducts is impractical.
How to Choose Detroit Radiant Products
Choosing the right Detroit Radiant heater starts with measuring the space's ceiling height and square footage. Infrared tube heaters and patio heaters are rated for different mounting heights and coverage areas. Contractors working in spaces without a gas line available should look at the electric infrared heater options instead of the gas-fired tube heaters.
For agricultural or industrial buildings, checking the heater's rated output against the building's heat loss calculation helps size the unit correctly rather than guessing based on square footage alone. Matching the heater's mounting configuration to the available ceiling or wall structure also avoids installation problems later.
Frequently Asked Questions
What brand name does Detroit Radiant use on its heaters?
Detroit Radiant Products Company sells its heating equipment under the Re-Verber-Ray brand name.
How long has Detroit Radiant been manufacturing heating equipment?
Detroit Radiant was founded in 1955 and has more than 70 years of manufacturing experience. The company still operates its own testing laboratory and tooling at its Warren, Michigan facility.
What types of spaces are Detroit Radiant infrared heaters designed for?
Detroit Radiant's infrared tube heaters and hot air unit heaters are built for commercial, industrial, and agricultural spaces. These include warehouses and large open buildings. The Designer Series patio heaters are built for outdoor comfort applications.
Does Detroit Radiant make anything besides heaters?
Detroit Radiant also manufactures process burners for industrial heating applications. Its Lumerica line covers industrial LED lighting fixtures. Contractors can combine heating and lighting purchases with a single manufacturer.
Where is Detroit Radiant based?
Detroit Radiant operates from Warren, Michigan, where it runs its manufacturing, testing laboratory, and tooling operations.