First Company began manufacturing HVAC equipment in 1966 and has built its reputation from a single Dallas, Texas facility ever since. The company operates a 900,000 square foot plant in Dallas and has shipped more than 5.5 million units since it opened its doors. First Company remains family owned, and several members of its production staff have more than 30 years of tenure with the company. Multi-occupant housing, hospitality properties, and commercial buildings across the country rely on equipment built at this single American facility.
Product Lines
First Company's product line centers on fan coils built for multi-occupant construction, including ceiling, wall mount, low height, and multi-position configurations for tight mechanical spaces. The ECO-Series covers packaged through-the-wall units that deliver conditioned air to individual rooms from a single outdoor connection, a common fit for hotel and apartment renovations. Water source heat pumps round out the lineup for buildings on closed loop or geothermal systems. Air handlers complete the catalog for larger commercial installations. Distributors, engineers, and contractors specify these products together when a multi-occupant building needs equipment sized room by room rather than one central system.
Why Contractors Specify First Company
Contractors working on hotel and apartment renovations specify First Company because its fan coils are engineered specifically for multi-occupant construction rather than adapted from single-family platforms. Multi-position fan coils let installers use the same base unit across ceiling, wall mount, and low height applications. This cuts down on how many part numbers a crew needs to stock across a large property. First Company's water source heat pump line lets contractors bid an entire building's mechanical system from a single manufacturer. First Company has also produced its equipment at one Dallas facility since 1966.
How to Choose First Company Products
Start by identifying the mechanical space in the unit, since First Company's ceiling, wall mount, low height, and multi-position fan coils are each sized for a different clearance. Match the coil capacity to the room's heating and cooling load rather than defaulting to a single tonnage across an entire property. Multi-occupant buildings often mix room sizes and exposures. For buildings on a shared water loop, confirm whether the system calls for a water source heat pump or a standard chilled water fan coil. The two use different piping configurations. Renovation projects that need to route conditioned air through an exterior wall are a good fit for the ECO-Series packaged units, which avoid extensive interior ductwork. Confirm voltage and electrical requirements against the mechanical drawings before ordering, since multi-occupant properties frequently mix single phase and three phase circuits across a building.
Frequently Asked Questions
What types of buildings use First Company fan coils?
First Company fan coils are built for multi-occupant construction such as hotels, apartments, and other multifamily properties, along with commercial buildings that need equipment sized room by room.
Where are First Company products manufactured?
First Company manufactures its products at a 900,000 square foot facility in Dallas, Texas, where the company has operated since 1966.
How do I choose between First Company's fan coil configurations?
First Company offers ceiling, wall mount, low height, and multi-position fan coils, each sized for a different clearance. Start by identifying the mechanical space in the unit. Multi-position fan coils let installers use the same base unit across ceiling, wall mount, and low height applications.
What are ECO-Series units used for?
ECO-Series units are packaged, through-the-wall HVAC systems that deliver conditioned air to a single room from one outdoor connection. They are a common choice for hotel and apartment renovations that need to avoid extensive interior ductwork.
Does First Company make equipment for water source heat pump systems?
Yes, First Company manufactures water source heat pumps for buildings on closed loop or geothermal systems, in addition to its fan coil and air handler lines.