Henry traces its roots to 1933 in Los Angeles. The company has spent over 90 years making building materials for waterproofing, roofing, and air and moisture control. It is now headquartered in El Segundo, California, with offices and manufacturing facilities across the United States and Canada.
In 2021, Henry became part of Carlisle Companies and today operates as a brand within Carlisle Weatherproofing Technologies. The company employs more than 2,500 people across 16 U.S. locations and 5 Canadian locations.
Product Lines
Henry's commercial product segment covers air and vapor barriers, polyiso insulation, roof coatings, roof membranes, single-ply roofing, waterproofing, and waterstops. The residential segment includes damp proofing, driveway maintenance products, housewraps, insulation, roof coatings, roofing underlayments, and window and door flashing.
An industrial segment rounds out the catalog with automotive coatings, marine sealants, paving products, polyurethane foams, and wax emulsions. This gives Henry a presence in building envelope work well beyond roofing alone.
Why Contractors Specify Henry
Henry markets its building envelope products as one system, with components tested and warranted to work together rather than mixed and matched from different manufacturers. That approach gives roofing and waterproofing contractors a single point of accountability when a warranty claim comes up.
The company has also picked up industry recognition for specific products. In 2025, it received an Architectural Record Product of the Year award for its UltraTouch recycled denim insulation. It also received an RCMA Project of the Year award in 2025 for restoration work at the New Orleans Convention Center.
How to Choose Henry Products
The starting point for selecting a Henry product is the segment: commercial, residential, or industrial. Commercial jobs typically draw from the roof membrane, roof coating, air/vapor barrier, and waterproofing lines. Residential jobs more often call for housewrap, roofing underlayment, or window and door flashing.
Henry positions its products as a matched system. Pairing components from the same product line, such as a roof membrane with its companion flashing and coating, keeps a job within the manufacturer's tested and warranted assembly. This avoids mixing components across unrelated lines.
Frequently Asked Questions
How long has Henry been making building materials?
Henry traces its history to 1933 in Los Angeles and has been producing building materials for more than 90 years.
Where is Henry headquartered?
Henry is headquartered in El Segundo, California, with additional offices and manufacturing facilities throughout the United States and Canada.
What kinds of products does Henry make for roofing contractors?
Henry's commercial line includes roof membranes, roof coatings, single-ply roofing, air and vapor barriers, waterproofing, and waterstops.
Is Henry an independent company?
No. Henry became part of Carlisle Companies in 2021 and now operates as a brand within Carlisle Weatherproofing Technologies.
Does Henry make products for residential jobs, not just commercial roofing?
Yes. Henry's residential line covers damp proofing, housewraps, insulation, roof coatings, roofing underlayments, and window and door flashing.