Jan-Air traces its history to Janette Manufacturing Company, founded in Chicago in 1909 to produce motors and blower wheels. In 1949 the fan division was purchased and relocated to Richmond, Illinois, operating from that point forward as Jan-Air, Inc. A fire destroyed most of the company's manufacturing facility in 1969, and Jan-Air rebuilt within a year at a new 20,000 square foot location rather than shutting down.
Ownership passed to Ken Bergsma and Ed Sattersten in 1974, and to current president Mark Sattersten in 2005. The company added a 12,000 square foot facility expansion in 2008 as part of ongoing modernization at its Richmond, Illinois plant. Jan-Air has stayed centered on centrifugal blower wheels and fans throughout that history, supplying OEMs, engineers, HVAC specialists, and contractors rather than shifting into unrelated product categories.
Product Lines
SupplyHouse carries Jan-Air's centrifugal blower wheels and fans along with related air-movement accessories. Jan-Air also builds custom OEM fan and blower solutions for equipment manufacturers whose applications fall outside standard catalog sizing. The company runs AMCA 210 flow meter testing capable of measuring performance up to 10,000 CFM. This gives it in-house verification of fan performance data rather than relying entirely on third-party testing.
Why Contractors Specify Jan-Air
HVAC and equipment technicians specify Jan-Air blower wheels and fans because the company's history is built around centrifugal air-movement components. It is not a broad catalog of unrelated HVAC parts. That focus matters when a replacement blower wheel needs to match the performance characteristics of the original component. Airflow and static pressure should stay within design tolerances after replacement. Jan-Air's in-house AMCA 210 testing capacity also gives contractors and OEMs a documented performance basis for a fan or blower wheel, rather than a spec sheet without verified backing.
How to Choose Jan-Air Products
Matching a Jan-Air blower wheel or fan to an application starts with confirming the airflow and static pressure requirements of the system it will serve. An undersized wheel will not move enough air, and an oversized one wastes energy and adds unnecessary noise. Contractors replacing an existing blower wheel should match wheel diameter, width, and rotation direction to the original component rather than assuming a similarly sized part will perform the same. For applications outside standard catalog sizing, such as specialized material handling or agricultural air-movement needs, Jan-Air's custom OEM solutions are more reliable than adapting a standard product to a nonstandard use.
Frequently Asked Questions
When was Jan-Air founded?
Jan-Air, Inc. was established in 1949 when the fan division of Chicago's Janette Manufacturing Company, founded in 1909, was purchased and relocated to Richmond, Illinois.
Did Jan-Air ever lose its manufacturing facility?
Yes. A fire destroyed most of the company's facility in 1969, and Jan-Air rebuilt within a year at a new 20,000 square foot location.
Who currently leads Jan-Air?
Mark Sattersten has served as Jan-Air's president since 2005, following ownership by Ken Bergsma and Ed Sattersten starting in 1974.
What products does Jan-Air manufacture?
Jan-Air manufactures centrifugal blower wheels and fans, air-movement accessories, and custom OEM fan solutions for equipment manufacturers.
How does Jan-Air verify its fan performance data?
Jan-Air runs AMCA 210 flow meter testing in-house, capable of measuring fan performance up to 10,000 CFM.