Klauber Machine and Gear Company, sold under the Klauber Gear name, has manufactured fractional horsepower gear motors since the 1950s from its facility in Pacific, Missouri. Now part of Global Point Technology Group, the company built its reputation supplying gear motors as an original equipment manufacturer to the RV, agricultural, and industrial equipment industries. Decades of OEM supply work mean the gear motor line was engineered to the tolerances larger manufacturers require, not adapted from a general purpose motor design.
Product Lines
Klauber Gear's catalog is organized around AC and DC fractional horsepower gear motors in three configurations. Parallel shaft in-line motors, covering the K100, K400, K440, K800, and K825 series, keep the output shaft aligned with the motor body for a compact footprint. Parallel shaft offset motors, including the K300, K350, K500, K600, and K900 series, move the output shaft to the side for applications where an in-line design won't fit. Right-angle gear motors in the K125, K150, and K175 series redirect output 90 degrees from the motor. The company also builds custom gear motors for applications the standard catalog doesn't cover.
Why Contractors Specify Klauber Gear
Contractors and equipment builders specify Klauber Gear motors when a project needs a gear motor sized and configured precisely rather than pulled from a generic catalog. The company has supplied gear motors as an OEM partner for decades, so its standard series already cover common mounting and shaft configurations. Equipment manufacturers rely on these configurations, which cuts down on custom engineering time. Klauber Gear motors are manufactured domestically in Pacific, Missouri.
How to Choose Klauber Gear Products
Selecting a Klauber Gear motor starts with the shaft configuration a project needs. Parallel shaft in-line models keep a compact straight line footprint. Parallel shaft offset models move the shaft to the side. Right-angle models redirect output 90 degrees. From there, matching horsepower and gear ratio to the load narrows the choice to a specific model. The K100 and K400 series differ from the higher capacity K800 and K825 series. For a project the standard catalog doesn't cover, a custom gear motor avoids forcing an off the shelf unit into an application it wasn't designed for.
Frequently Asked Questions
When was Klauber Gear founded?
Klauber Machine and Gear Company was founded in the 1950s and has manufactured fractional horsepower gear motors ever since.
Where are Klauber Gear motors manufactured?
Klauber Gear motors are manufactured in Pacific, Missouri.
What shaft configurations does Klauber Gear offer?
Klauber Gear offers parallel shaft in-line, parallel shaft offset, and right-angle gear motor configurations.
Does Klauber Gear build custom gear motors?
Yes, Klauber Gear builds custom gear motors for applications that fall outside its standard parallel shaft and right-angle series.
What industries does Klauber Gear primarily serve?
Klauber Gear supplies gear motors as an OEM to the RV, agricultural, and industrial equipment industries.