MAMAC Systems got its start in the early 1980s. Its founder began applying microcomputers to automate HVAC and environmental control systems, an approach the industry hadn't widely adopted at the time. The company has marketed itself as a pioneer in green building technology since 1980, building its business around cutting energy waste in commercial and institutional buildings.
MAMAC Systems now operates as a global manufacturer. Its customers and distribution reach North America, Europe, and Asia. Operations are based in Minneapolis, Minnesota, Canada, Singapore, and the United Kingdom.
Product Lines
MAMAC Systems builds sensors, transducers, and control peripherals. They are used across HVAC and environmental control systems, remote monitoring, alarming, and energy metering applications. Its catalog includes temperature sensors for duct, immersion, and outdoor air applications. It also includes current sensors and pressure transducers used to monitor airflow, refrigerant, and hydronic systems.
The company also supplies a line of sensor and control peripherals, the wiring accessories and mounting hardware installers need to get a sensor connected into a building automation system.
Why Contractors Specify MAMAC Systems
Contractors and controls technicians turn to MAMAC Systems when a building automation job calls for a sensor built specifically for HVAC and energy-metering duty rather than a generic industrial part. The company's catalog spans temperature, current, and pressure sensing, along with the peripherals that connect them. A technician can often source an entire measurement point from one manufacturer instead of piecing components together from several suppliers.
MAMAC's decades-long focus on HVAC and environmental controls also means its sensor lines are built around the voltage ranges, mounting styles, and output signals that building automation panels expect. This cuts down on compatibility guesswork during installation.
How to Choose MAMAC Systems Products
Selecting the right MAMAC sensor starts with the measurement point. Airflow and refrigerant work calls for a pressure transducer, while monitoring space, duct, or outdoor air conditions calls for one of MAMAC's temperature sensors.
Current sensors fit best where a technician needs to confirm that a motor, pump, or compressor is actually running rather than relying on a control signal alone. This is useful for alarming and fault detection. The next step is matching the sensor's output signal and voltage range to the building automation panel it will connect to. For less standard sensing needs, MAMAC's sensor and control peripherals line fills in the wiring accessories and mounting hardware a straightforward installation still requires.
Frequently Asked Questions
When was MAMAC Systems founded?
MAMAC Systems traces its history back to 1980, when its founder began using microcomputers to automate HVAC and environmental control systems.
What kind of products does MAMAC Systems make?
MAMAC Systems manufactures sensors, transducers, and control peripherals. These serve HVAC and environmental controls, remote monitoring, alarming, and energy metering.
Where does MAMAC Systems operate?
MAMAC Systems serves customers across North America, Europe, and Asia, with operations based in Minneapolis, Minnesota, Canada, Singapore, and the United Kingdom.
What's the difference between a MAMAC current sensor and a pressure transducer?
A current sensor confirms that a motor, pump, or compressor is drawing power and running. A pressure transducer measures airflow, refrigerant, or hydronic pressure at a specific point in the system.
Does MAMAC Systems sell mounting hardware for its sensors?
Yes, the company's sensor and control peripherals line covers the wiring accessories and mounting hardware installers need to put a sensor into service.