Mammoth traces its roots to 1935, when the company began building custom HVAC equipment for commercial and institutional projects. Today the brand operates as part of Nortek Air Solutions, headquartered in Okarche, Oklahoma, with equipment manufactured at a dedicated facility in St-Leonard-D'Aston, Quebec, Canada.
Mammoth built its business around custom-packaged direct expansion systems. They serve architects, engineers, contractors, and building owners who need equipment matched to a specific commercial application rather than an off-the-shelf unit. The brand designs its systems with energy efficiency and acoustic performance as priorities. Its equipment can be configured to support LEED certification requirements on qualifying projects.
Product Lines
Mammoth's core product line centers on the Ultraline custom packaged rooftop system, a factory-packaged direct expansion unit with integrated factory controls built for commercial rooftop installations. Much of the commissioning work on an Ultraline unit is completed before it leaves the factory, which shortens the setup work still needed on site.
The V-Cube vertical self-contained system and its V-Cube Slim variant give specifiers an indoor alternative to a rooftop package. Both suit applications where vertical mechanical room space is available. They fit where roof loading, access, or penetrations rule out a curb-mounted unit. The Slim version is trimmed for narrower mechanical rooms.
Why Contractors Specify Mammoth
Contractors and mechanical engineers turn to Mammoth when a project calls for equipment built to the job rather than a stock model pulled from a shelf. Because Mammoth packages systems to order, a specifier can call out capacity, controls, and acoustic treatment. These match the building's actual load and site constraints. The building does not have to adapt to a standard unit.
Such flexibility matters most on retrofit and replacement jobs, where existing curb dimensions, electrical service, or ductwork limit what equipment will physically fit. Mammoth's factory-installed controls also arrive pre-wired and configured, cutting down the amount of controls work a contractor has to complete after the unit is set.
How to Choose Mammoth Products
Selecting the right Mammoth system starts with available space and access. A rooftop location with structural capacity for a curb-mounted unit points toward the Ultraline custom packaged rooftop system, which handles higher-capacity commercial loads in a single weatherproof package.
When roof access or structural loading rules out a rooftop unit, the V-Cube vertical self-contained system offers an indoor alternative that ties into ductwork without requiring roof penetrations. Buildings with tight mechanical room footprints should look at the V-Cube Slim variant, which trims the cabinet depth for narrower spaces. Specifying acoustic and efficiency options up front, rather than after the order is placed, keeps the unit sized correctly for both the load and the building's noise requirements.
Frequently Asked Questions
When was Mammoth founded?
Mammoth traces its history back to 1935, when it began building custom HVAC equipment for commercial projects.
Who manufactures Mammoth HVAC equipment?
Mammoth operates as a brand of Nortek Air Solutions, headquartered in Okarche, Oklahoma, with equipment manufactured at a facility in St-Leonard-D'Aston, Quebec, Canada.
What's the difference between the Ultraline and V-Cube product lines?
The Ultraline is a custom packaged rooftop direct expansion system, while the V-Cube is a vertical self-contained system built for indoor installation instead of a roof curb.
Is the V-Cube Slim different from a standard V-Cube unit?
Yes, the V-Cube Slim uses a narrower cabinet than the standard V-Cube, which helps it fit into mechanical rooms with limited depth.
Can Mammoth equipment support LEED certification goals?
Mammoth designs its systems with energy efficiency and acoustic performance in mind, and equipment can be configured to support LEED certification requirements on qualifying projects.