Apply to be a TradeMaster!
Main product image of Noritz Connect Wi-Fi Adapter
Magnifying glass
Hover image to zoom

Noritz Connect Wi-Fi Adapter

Brand:
Noritz
SKU:
NWC-ADAPTER
Rating:
(7)
Q&A:
(0)
Noritz Connect Wi-Fi Adapter
Magnifying glass
Hover image to zoom
$227.84 each
In Stock
In Stock
Get 1 Tomorrow, Nov 19
Order by 6PM, receive Tomorrow
Free Shipping This item ships free
Easy Returns No restocking fee for 90 days

Description

–
Noritz Tankless Technology now has the option to become even smarter with the new Wi-Fi Adapter!

Features
  • The easy-to-install adapter is weatherproof and can be outdoors.
  • Noritz Connect - Mobile App - Convenient wireless control at your fingertips. Anytime. Anywhere.
  • Wireless Control - Homeowners can now control heater functions over the new full featured app.
  • Diagnose and Maintain - Homeowner alerts and reminders for fast and proactive maintenance.
  • Flexible Installation - Weather resistant Wi-Fi adapter for installation indoors or outdoors.
  • Noritz Connect app available for download from the Apple App Store & Android's Google Play.
Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


Product Reviews

4.43 out of 7 reviews
86% would recommend this product
4.43
out of 7 Reviews
86% would recommend this product
WRITE A REVIEW
5 star
57%
4 star
29%
3 star
14%
2 star
0%
1 star
0%
WRITE A REVIEW
Showing 1-7 of 7 reviews

Doesn't do what I had hoped

No issues with Supply House. I get my orders quickly and at a good price. However, this product from Noritz just doesn't do much. I read that prior to purchasing and called Noritz directly to find out if it would allow me to control my circulation pump and set my time on the unit. At least at this point I am finding the software to be very quirky with delays to connect. Once connected I don't have any real control of the unit and definately can't figure out how to control the recirc pump. Unit physically connected fine but how it operates really is an issue. I cannot recommend buying this unit but that may change once I work with Noritz to get more clarity on why my unit isn't allowing me to control the unit as their sales people told me it would.
StevieG
Tennessee
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Supply house is great

The connector does work, it's a bit of a pain to configure the wifi, not as seemless as some smart devices and it requires a strong wifi signal which is a problem for basement. But the product is the manufacturer standard product and comes with the cable connection.
J
Portland, OR
6 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Not necessary but convenient

So the Noritz Wi-Fi Adapter like most other smart home wifi products are not really necessary but they are definitely nice to haves as we start evolving our homes. This adapter does pretty much the same thing as the wired remote that comes with the unit does but I can conveniently do it from my phone from anywhere. Lets say I forgot to turn off the unit before leaving for a vacation or need to turn up the temp while cooking, etc, I can do so from my phone. It also has maintenance reminders which is great because it's 1 less thing to think about.
Johnny the Walker
Los Angeles, CA
6 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Practical and convenient access for control and usage status

Is good to know that things are working the way it should and this remote helps you do exactly that! Installation for the device and wire connections were simple and quick. The iOS/Android app is easy to install, but it is hard to configure. Be warned that more than one attempt will be needed to get it all working correctly. One word of advice; do follow the instructions completely and things will work out faster! Once configured, the app does take no less than 48 hours to show its initial usage stats. I would add that Noritz still has some way to go optimizing the app. For example, things like editing the schedule for descaling and doing other maintenance or preventive services are clearly not there yet in the app. Configuring alerts are also missing which forces you to access the app whenever you want to figure out if everything is working ok or not. All in all... It's a first step! It's nice that you don't have to walk up to the water heater to make any adjustment or reset the unit.
bermudan
McKinney TX
6 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Your service was very good and the price was lower.

The parts fit without any issues and the system is working flawlessly.
Perry
Arlington, NE
7 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Fast delivery and great price

3rd time using Supply House and very happy.
Steve
San Rafael, CA
8 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works great, wish they had thought install out better

The WiFi adaptor does what is is supposed to but it is frustrating that you have to install the remote control panel and then the WiFi as opposed to just the WiFi adaptor. While it is nice to have local control without WiFi it is a duplicate cost.
Sealwrangler
San Francisco, CA
8 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy