PhazPak manufactures phase converters that let three-phase motors and equipment run on a single-phase power supply. The company is based in Monroe, Indiana, and has built solid-state phase converters for more than 15 years and rotary phase converters for more than 40 years.
PhazPak's core customers are contractors and equipment owners. They need to run three-phase machinery, such as pumps or shop equipment, where only single-phase electrical service is available. The company offers both solid-state and rotary converter technologies, giving installers a choice between the two approaches depending on the load and application.
Product Lines
PhazPak's solid-state phase converters are built for lighter-duty or intermittent loads, offering a more compact option than a rotary converter for equipment that does not run continuously. Its rotary phase converters, a product line the company has manufactured for more than 40 years, are suited to heavier and continuous-duty three-phase loads.
Both converter lines are designed as complete, packaged units meant to simplify installation compared to building a custom phase-conversion setup on site. PhazPak sells its converters through a distributor network rather than only direct to end users.
Why Contractors Specify PhazPak
Contractors specify PhazPak converters on jobs where three-phase equipment must run at a site with only single-phase power. This is common in rural locations, older commercial buildings, and residential properties with shop equipment or well pumps. PhazPak has manufactured rotary converters for more than 40 years and solid-state converters for more than 15. Contractors have a long track record to reference when matching converter type to load.
Offering both solid-state and rotary technology under one brand lets a contractor select the right converter type for the specific load instead of relying on a single conversion method. Packaged units also reduce on-site assembly time compared to building a custom conversion setup, which matters on jobs where downtime for the three-phase equipment needs to stay short.
How to Choose PhazPak Products
Match the converter type to how the three-phase load runs. Solid-state converters suit lighter, intermittent-duty equipment, while rotary converters are built for heavier, continuous-duty loads. Confirm the horsepower or amperage draw of the three-phase equipment before selecting a converter size, since undersizing a converter can prevent the equipment from starting or running correctly.
For equipment that runs most of the day, such as a well pump or shop compressor, a rotary converter is typically the better match given its continuous-duty design. For equipment used only occasionally, a solid-state converter can be a more compact option. Verify that the available single-phase voltage and amperage at the site match PhazPak's input requirements for the converter model under consideration.
Frequently Asked Questions
What does a PhazPak phase converter do?
A PhazPak phase converter lets three-phase motors and equipment run on a single-phase electrical supply, which is useful at sites that do not have three-phase power available.
What is the difference between PhazPak's solid-state and rotary converters?
Solid-state converters are built for lighter, intermittent-duty loads and a more compact footprint, while rotary converters are designed for heavier, continuous-duty three-phase loads.
How long has PhazPak manufactured phase converters?
PhazPak has manufactured rotary phase converters for more than 40 years and solid-state phase converters for more than 15 years.
Where is PhazPak based?
PhazPak is headquartered in Monroe, Indiana.
What kind of equipment typically needs a PhazPak converter?
Three-phase equipment such as well pumps, shop compressors, and other motor-driven machinery typically needs a phase converter when installed at a site with only single-phase power available.