Phoenix Manufacturing has spent over 50 years focused on evaporative cooling equipment and replacement parts, building its business around the swamp cooler technology common in hot, dry climates. The company is based in Phoenix, Arizona, putting it close to the desert Southwest market where evaporative cooling is a primary form of home and commercial comfort cooling.
That regional focus shows up in Phoenix Manufacturing's product catalog. It stays centered on evaporative cooler motors, blower wheels, and cooling media rather than branching into compressor-based air conditioning or heating equipment.
Product Lines
SupplyHouse carries Phoenix Manufacturing OEM motors, including 115V models such as the 05-007-0035 and 05-007-0133. It also carries blower wheels like the 05-003-0035 and sleeve bearing sets such as the 05-003-0064. These parts are used to service evaporative coolers already in the field.
Phoenix Manufacturing's broader lineup includes Frigiking window and blower coolers that use aspen cooling media. It also includes AeroCool coolers built around rigid media. Commercial evaporative units are rated up to 22,000 CFM for warehouses, schools, and other large spaces.
Why Contractors Specify Phoenix Manufacturing
Technicians who service evaporative coolers regularly need motors, blower wheels, and bearing sets that match the physical dimensions and mounting pattern of the original equipment. Phoenix Manufacturing's OEM parts are built to fit its own cooler lines without modification.
Phoenix Manufacturing offers aspen media coolers under the Frigiking name and rigid media coolers under the AeroCool name. Contractors working across a range of installed units can source replacement media and motors from one brand, regardless of which media type a given cooler uses.
How to Choose Phoenix Manufacturing Products
Match the exact motor part number, such as the 05-007-0035 or 05-007-0133, to the horsepower and voltage rating stamped on the original motor. Do not substitute by horsepower alone, since mounting dimensions vary across Phoenix Manufacturing's motor lineup.
Confirm whether the installed cooler uses aspen media or rigid media before ordering replacement pads. Frigiking units are built around aspen media, while AeroCool units use rigid media. The two are not interchangeable in the same cooler housing.
Frequently Asked Questions
What does Phoenix Manufacturing make?
Phoenix Manufacturing makes evaporative coolers and replacement parts for residential and commercial applications. The parts include motors, blower wheels, bearing sets, and cooling media.
Where is Phoenix Manufacturing based?
Phoenix Manufacturing is based in Phoenix, Arizona, and has focused on evaporative cooling equipment for over 50 years.
What is the difference between Frigiking and AeroCool coolers?
Frigiking coolers use aspen cooling media, while AeroCool coolers are built around rigid media, so replacement media is not interchangeable between the two lines.
How do I know which Phoenix Manufacturing motor to order?
Match the exact part number, such as the 05-007-0035 or 05-007-0133, along with the horsepower and voltage stamped on the original motor, since mounting dimensions vary across the lineup.
Does Phoenix Manufacturing make coolers for commercial buildings?
Yes. Phoenix Manufacturing offers commercial evaporative coolers rated up to 22,000 CFM for warehouses, schools, and similar large spaces.