Toilet Master is a line of plumbing specialty tools made by Junca Inventions Unlimited, built around a single job: removing and resetting toilets without lifting them by hand.
The lineup stays narrow and purpose-built rather than spanning general plumbing tools.
Product Lines
The core product is the Toilet Master Jack, a mechanical lifting tool that raises and moves a toilet during installation or repair work. Toilet Master Bolts, described as a metal, break-resistant design, cover the mounting hardware side of the same job.
Replacement parts for the jack are sold separately, so a worn component does not force a contractor to replace the whole tool.
Why Contractors Specify Toilet Master
Repeated toilet lifting is a common source of back strain on plumbing crews, and a mechanical jack removes that lift from the job entirely. All-swivel casters make the tool maneuverable in tight bathroom spaces. Protective covering on the parts that contact the toilet reduces the chance of chipping or scratching fixtures during the move.
At roughly 20 pounds, the jack is light enough to carry between job sites in a service vehicle without dedicating significant cargo space to it.
How to Choose Toilet Master Products
Crews doing frequent toilet removal and reset work, such as flooring or plumbing repair specialists, get the most use out of the jack itself. Bolt kits should match the toilet's mounting pattern and floor flange type.
Shops that put the jack into daily rotation should keep replacement parts on hand. A single worn caster or lift component can otherwise sideline the whole tool.
Frequently Asked Questions
What does the Toilet Master Jack do?
It is a mechanical tool that lifts and moves a toilet during installation or repair, so installers do not have to lift the fixture by hand.
Who manufactures Toilet Master products?
Toilet Master products are made by Junca Inventions Unlimited.
Are Toilet Master Bolts different from standard toilet bolts?
Toilet Master describes its bolts as a metal, break-resistant design.
How much does the Toilet Master Jack weigh?
The jack weighs about 20 pounds, which makes it light enough to carry between job sites.
Are replacement parts available for the Toilet Master Jack?
Yes, replacement components are sold separately from the full jack.