Topog-E is a gasket manufacturer founded in 1956 to build a rubber alternative to the fibrous boiler gaskets common at the time. The company is headquartered in Cibolo, Texas, where it still manufactures its proprietary rubber compound in-house rather than outsourcing production. Topog-E produces roughly one million gaskets per year across more than 300 sizes, supplying boiler and steam system components to the HVAC and mechanical trades. Its original rubber gasket design remains the foundation of the current product catalog.
Product Lines
SupplyHouse carries Topog-E's core Series 180 molded rubber gaskets, the company's original product line built for boiler applications. The catalog also includes Series 450 gaskets made from tacky cloth with an elastomer compound. Series 1000 and 2000 are high-temperature graphite gaskets for more demanding steam and pressure applications. For high-pressure needs, Topog-E's Series 3000 and 3000ET lines use expanded PTFE construction. Beyond these core series, the company also manufactures ANSI flange gaskets, mechanical packings, spiral wound gaskets, and related sealing components for steam, air, and water systems.
Why Contractors Specify Topog-E
Contractors specify Topog-E because the company has manufactured boiler gaskets continuously since 1956. Because Topog-E makes its own rubber compound in-house rather than sourcing it from a third party, the company controls consistency across its full range of sizes. The tiered product lines run from standard molded rubber up through high-temperature graphite and expanded PTFE. They let a contractor match gasket material to the specific pressure and temperature demands of a job. This avoids over-specifying a premium gasket for a routine repair. Producing about one million gaskets a year also means common sizes stay available for time-sensitive boiler service calls.
How to Choose Topog-E Products
Start by confirming the boiler make and model so the gasket matches the flange dimensions exactly, since a mismatched gasket can affect the seal. For standard steam boiler service, the Series 180 molded rubber gasket covers most routine replacement jobs. Higher-temperature or higher-pressure applications call for the Series 1000 or 2000 graphite gaskets. The Series 3000 and 3000ET expanded PTFE lines suit high-pressure systems that exceed standard rubber gasket limits. For non-boiler sealing needs, check whether an ANSI flange gasket, mechanical packing, or spiral wound gasket better fits the application before defaulting to a boiler-specific series.
Frequently Asked Questions
What does Topog-E manufacture?
Topog-E manufactures rubber and specialty gaskets for steam boilers, along with related sealing components for air and water systems.
When was Topog-E founded?
Topog-E was founded in 1956 to develop a rubber alternative to fibrous boiler gaskets.
Where is Topog-E headquartered?
Topog-E is headquartered in Cibolo, Texas, where it manufactures its gaskets and proprietary rubber compound.
What is the difference between Topog-E's Series 180 and Series 3000 gaskets?
Series 180 is a standard molded rubber gasket for routine boiler service, while Series 3000 and 3000ET use expanded PTFE for high-pressure applications.
Does Topog-E make anything besides boiler gaskets?
Yes, the company also manufactures ANSI flange gaskets, mechanical packings, spiral wound gaskets, and other sealing components.