Yaskawa Electric was established in 1915 in Japan and has grown into one of the world's largest manufacturers of AC inverter drives, servo systems, and motion control equipment. Yaskawa America handles drives and motion products for the Americas from its headquarters in Waukegan, Illinois. The company has built variable frequency drives for building automation and HVAC systems for more than 30 years, alongside its industrial drive and robotics lines. Contractors and engineers working on commercial mechanical systems typically encounter Yaskawa through its HVAC drive line rather than its broader industrial or robotics catalog.
Product Lines
Yaskawa's HVAC drives are built specifically for fan, pump, and compressor applications in commercial building automation systems, with the HV600 representing the company's newest drive in that line. The broader industrial AC drive catalog includes general purpose drives and microdrives that also see use in mechanical rooms running fans and pumps outside a full building automation setup. Yaskawa also manufactures medium voltage drives for larger commercial and industrial installations where standard low voltage drives cannot handle the load. Motion control products, including Sigma series servo motors, serve manufacturing and industrial automation rather than HVAC and plumbing trades. Yaskawa's robotics lines serve manufacturing and industrial automation as well.
Why Contractors Specify Yaskawa
Mechanical contractors specify Yaskawa drives on building automation projects. The company has supported building automation and HVAC systems for more than three decades. That gives its HVAC drive line a long track record on commercial fan and pump applications. Facility engineers managing energy costs use variable frequency drives to ramp motor speed to actual demand instead of running fans and pumps at a fixed speed. Yaskawa's HVAC drive line, including the HV600, is built specifically for that role. Contractors who handle both HVAC and general industrial motor control work also gain from sourcing drives across both categories from a single manufacturer.
How to Choose Yaskawa Products
Confirm whether the application is building automation and HVAC specific or general industrial motor control, since Yaskawa splits its drive catalog along those lines and each is optimized differently. Size the drive to the motor's horsepower and voltage rather than rounding up. Check whether the installation needs a low voltage or medium voltage drive based on the building's electrical service. For projects tied into a building automation system, confirm the drive model supports the building's existing automation setup before ordering. Not every Yaskawa drive ships with the same communication options. Motion control and servo products are built for manufacturing and industrial automation, not HVAC or plumbing applications. Contractors on commercial mechanical jobs should stay within the HVAC and industrial AC drive lines.
Frequently Asked Questions
What is the difference between Yaskawa's HVAC drives and its industrial AC drives?
Yaskawa's HVAC drives are built specifically for fan, pump, and compressor applications in building automation systems. Its industrial AC drive line, including general purpose drives and microdrives, covers broader motor control applications outside of HVAC.
Where is Yaskawa America headquartered?
Yaskawa America is headquartered in Waukegan, Illinois. It handles drives and motion products for the Americas.
How long has Yaskawa made HVAC drives?
Yaskawa has more than 30 years of experience building variable frequency drives for building automation and HVAC systems, with the HV600 as its newest drive in that line.
When was Yaskawa Electric established?
Yaskawa Electric was established in Japan in 1915.
Does Yaskawa make medium voltage drives for large commercial buildings?
Yes, Yaskawa manufactures medium voltage drives for commercial and industrial installations where a standard low voltage drive cannot handle the load.