iFLO Pro is a drain pan treatment brand headquartered in Miramar, Florida, and operated by Great Innovations, LLC. The company builds its lineup around one specific field problem: zooglea bacteria buildup in HVAC condensate drain pans. This buildup is a leading cause of clogged drain lines and water damage callbacks.
The brand sells exclusively through wholesale distribution to licensed HVAC contractors rather than directly to homeowners, and it backs its devices with a certification program for installer partners. iFLO Pro reports its devices are active in more than 55,000 installed units.
Product Lines
The core of the iFLO Pro lineup is its device family, sold in Basic, Mini, and Battery models. Each is built to dose a bio-enzymatic formula directly into the drain pan on a set schedule. The formula itself is sold separately in 36 ounce and 72 ounce bottles sized for six month or one year supply periods.
iFLO Pro also offers an admin dashboard for monitoring device status and float switch alerts remotely. Contractors can track drain pan conditions across a customer base without a truck roll for every check.
Why Contractors Specify iFLO Pro
Contractors specify iFLO Pro because its enzyme-based formula is designed to break down zooglea bacteria in about eight hours, compared to roughly 72 hours for typical consumer-grade drain treatments. Faster breakdown means fewer emergency calls for a clogged condensate line and less risk of a shutoff switch tripping the system.
The formula is built to be non-toxic and non-corrosive to the metals and equipment inside an air handler. This matters on service calls in occupied spaces, where a contractor can't risk damaging the coil or pan.
How to Choose iFLO Pro Products
Match the device model to the install. The Battery model suits drain pans without easy access to line voltage. The Basic and Mini models are sized for standard residential and light commercial air handlers. Order the 36 ounce bottle for a six month service interval or the 72 ounce bottle for a full year. Base that choice on how often a technician can realistically get back to the site.
Contractors managing several accounts should weigh the admin dashboard option. Remote float switch alerts let a technician prioritize which drain pans need attention before a callback comes in rather than after.
Frequently Asked Questions
What problem does iFLO Pro solve?
It treats zooglea bacteria buildup in HVAC condensate drain pans, which is a common cause of clogged drain lines and water damage.
How fast does the iFLO Pro formula work?
The formula is built to break down zooglea bacteria in about eight hours, compared to roughly 72 hours for typical consumer-grade treatments.
Is iFLO Pro sold to homeowners directly?
No. iFLO Pro sells exclusively through wholesale distribution to licensed HVAC contractors.
What device models does iFLO Pro offer?
The lineup includes Basic, Mini, and Battery models, each built to dose the drain pan formula on a set schedule.
Is the iFLO Pro formula safe around HVAC equipment?
The formula is designed to be non-toxic and non-corrosive to the metals and equipment inside an air handler.