AstroShield reflective insulation comes from Innovative Energy Inc., a family-owned manufacturer founded in 1980 by Bob Wadsworth. The company grew out of a 1978 solar greenhouse project, after Wadsworth found that reflective materials held collected heat better than mass insulation products did. Innovative Energy started on the Wadsworth family farm and moved to a larger facility in Lowell, Indiana in 1995 to keep up with demand. Headquartered in Crown Point, Indiana, the company has stayed in the family since Wadsworth's daughter Whitney and her husband Jonathon Hagarbome took over ownership in 2019.
Product Lines
Innovative Energy sells AstroShield insulation in several configurations. AstroShield I sandwiches a single bubble layer between two metalized sheets at roughly 3/16 inch thick. AstroShield II doubles that to two bubble layers between metalized sheets at about 5/16 inch. White-faced versions of each, AstroShield White I and White II, swap the metalized film on one side for a white finish. SupplyHouse stocks the R-6 rated duct-insulation version of this line in rolls such as the 48-inch by 125-foot AHD48X125 and the 60-inch by 100-foot AHD60X100. Innovative Energy's broader catalog also includes AstroScrim and Astro-Armour building insulation. Other products include R+Heatshield radiant barrier, Tuff-Stuff insulation, and Arctic Package insulation for fleet and RV use.
Why Contractors Specify AstroShield
Installers use AstroShield because its reflective surfaces block about 95 percent of radiant heat transfer when installed with the recommended air space. It replaces separate vapor barrier, air infiltration barrier, and insulation layers with a single product. Combining those three layers into one material cuts down on what a crew has to carry and install on a duct run or wall assembly. The metalized polyester film surface also holds up to the folding, cutting, and handling that comes with a typical HVAC or construction install.
How to Choose AstroShield Products
Layer count and thickness are the main variables. AstroShield I uses a single bubble layer at about 3/16 inch thick. AstroShield II doubles that to two bubble layers at roughly 5/16 inch for a higher R-value. Facing color matters for visible installations, since the White I and White II versions swap the metalized film on one exposed side for a white finish. For duct runs specifically, SupplyHouse carries the R-6 rated AstroShield II duct insulation in set roll widths like 48 inches and 60 inches. Measuring the duct run length and diameter ahead of time helps avoid ordering the wrong size.
Frequently Asked Questions
Who manufactures AstroShield insulation?
AstroShield comes from Innovative Energy Inc., a family-owned manufacturer founded in 1980 and headquartered in Crown Point, Indiana.
What's the difference between AstroShield I and AstroShield II?
AstroShield I uses a single bubble layer between two metalized sheets at about 3/16 inch thick. AstroShield II doubles that to two bubble layers at roughly 5/16 inch, giving it a higher R-value for duct and building insulation applications.
How much radiant heat does AstroShield block?
Innovative Energy states that AstroShield's reflective surfaces block about 95 percent of radiant heat transfer when installed with the recommended air space.
Was AstroShield previously sold under a different name?
AstroShield is Innovative Energy's updated version of its earlier Astro-Foil insulation, built with an improved surface layer.
What duct insulation sizes does SupplyHouse carry?
SupplyHouse stocks AstroShield II R-6 duct insulation in rolls including the 48-inch by 125-foot AHD48X125 and the 60-inch by 100-foot AHD60X100.