Kelvion is a German manufacturer that describes itself as the leading global developer and manufacturer of heat exchange solutions. The company operates through a global sales, service, and production network that supports customers across a wide range of thermal management applications.
Kelvion's engineering focus spans HVAC and refrigeration equipment, power generation, and heavy industrial processes. That gives the brand a broader technical base than manufacturers that build heat exchangers for a single market segment.
Product Lines
Kelvion's catalog covers plate heat exchangers in brazed, gasketed, and welded configurations. It also includes evaporators and air coolers built for refrigeration and cooling loads. The company also manufactures heat rejection and heat recovery systems for facilities looking to capture and reuse thermal energy from existing processes.
Beyond core HVAC and refrigeration equipment, Kelvion produces heating solutions and process heat transfer products. Its lineup also includes engine and generator cooling systems and transformer cooling equipment. That range lets contractors and engineers source multiple types of heat exchange equipment from a single manufacturer rather than piecing together components from several vendors.
Why Contractors Specify Kelvion
Mechanical contractors and engineers specify Kelvion equipment because the product range covers standard HVAC and refrigeration duty. It also covers more demanding industrial thermal loads. A firm that mixes commercial refrigeration work with heavier process or power applications can standardize on one manufacturer instead of qualifying multiple heat exchanger suppliers.
Kelvion also serves markets that require heat exchange equipment built for continuous industrial use. These include power and energy, chemicals, and oil and gas applications. Specifying a brand with that industrial pedigree gives contractors confidence the equipment is built for demanding duty cycles, not just light commercial service.
How to Choose Kelvion Products
Selecting the right Kelvion heat exchanger starts with matching the plate configuration to the application. Brazed plate heat exchangers suit compact installations with lower serviceability needs, while gasketed plate units make sense where a system needs to be opened for cleaning or plate replacement. Welded plate heat exchangers fit applications involving more aggressive fluids or higher pressure and temperature requirements.
For refrigeration and cooling work, size evaporators and air coolers to the specific cooling load. Match them to the refrigerant type in use. Facilities pursuing energy recovery should look at Kelvion's heat rejection and heat recovery lines, which are built to capture waste heat rather than simply reject it. Matching the equipment category to the actual thermal duty, rather than defaulting to a familiar model, keeps the system running at its intended efficiency.
Frequently Asked Questions
What types of heat exchangers does Kelvion manufacture?
Kelvion manufactures brazed, gasketed, and welded plate heat exchangers. It also makes evaporators, air coolers, heat rejection and recovery systems, and process heat transfer equipment.
Does Kelvion only serve HVAC and refrigeration applications?
No. Kelvion also serves heavy industrial markets beyond HVAC and refrigeration. These include power and energy, chemicals, oil and gas, and transportation.
When should a gasketed plate heat exchanger be used instead of a brazed one?
Gasketed plate heat exchangers make sense when a system needs to be opened periodically for cleaning or plate replacement, while brazed units suit compact installations with lower serviceability needs.
What is the difference between heat rejection and heat recovery equipment?
Heat rejection equipment discharges waste heat from a system, while heat recovery equipment is built to capture and reuse that thermal energy elsewhere in a facility.
Is Kelvion equipment suited for higher-pressure or higher-temperature systems?
Welded plate heat exchangers in Kelvion's lineup are built for applications involving more aggressive fluids or higher pressure and temperature requirements than standard gasketed units handle.