Linear-X is a hydronic manifold actuator and control brand operated as a division of Ultra-Fin MFG. The product line centers on a single, focused idea. One all-in-one operating system replaces multiple individual thermal actuators on a hydronic manifold and controls every valve from a single unit.
The Linear-X system is built around on/off actuator technology rather than the continuously powered thermal actuators common on hydronic manifolds. The actuators power down once a valve reaches its open or closed position instead of staying energized. The manufacturer states this can cut actuator energy use by up to 99 percent compared to standard thermal actuators. That claim matters most on multi-zone systems, where several actuators would otherwise run continuously.
Product Lines
SupplyHouse carries Linear-X operating systems across a range of valve counts, from four valves up to twelve. Installers can match the unit to the number of zones on a given hydronic manifold. Each unit is designed to work with manifolds using 50 millimeter or 2 inch branch spacing. This is the standard spacing used across most hydronic manifold brands, so the product is not locked to a single manifold manufacturer.
Why Contractors Specify Linear-X
Hydronic installers specify Linear-X on multi-zone jobs because one control unit reduces the number of individual components that can fail or need service. A bank of separate thermal actuators has more of them. The plug and play installation approach also matters on retrofit jobs. Minimizing time spent rewiring or reconfiguring an existing manifold setup keeps a service call from turning into a full system replacement. Because the actuators are not continuously powered, contractors can offer Linear-X as a direct fix on systems where actuator noise or heat buildup has been a complaint.
How to Choose Linear-X Products
Choosing the correct Linear-X unit starts with counting the valves on the hydronic manifold that need control. Each model is built for a specific valve count, and units are not designed to be daisy-chained past their rated capacity. Before ordering, installers should also confirm that the manifold's branch spacing matches the 50 millimeter or 2 inch standard the Linear-X system is built around. A mismatch means the actuator hardware will not seat correctly. On jobs with more zones than the largest available Linear-X unit supports, installers need to plan for multiple units rather than assuming one system will scale indefinitely.
Frequently Asked Questions
What is Linear-X?
Linear-X is a hydronic manifold actuator and control system, operated as a division of Ultra-Fin MFG, that manages every valve on a manifold from one unit.
How much energy does Linear-X claim to save compared to standard thermal actuators?
The manufacturer states the system can save up to 99 percent of the energy used by standard thermal actuators. Its actuators power down once a valve reaches position instead of staying continuously energized.
What valve counts does Linear-X come in?
Linear-X actuator systems are available in valve counts ranging from four to twelve to match different hydronic manifold sizes.
Does Linear-X work with every hydronic manifold?
Not with every manifold. Linear-X is built for manifolds using 50 millimeter or 2 inch branch spacing. This is the standard spacing used across most hydronic manifold brands.
Is Linear-X installation complicated?
No. The system is designed for plug and play installation, intended to install in minutes rather than requiring extensive rewiring.