Micro-Air, based in Hamilton, New Jersey, designs soft starters and control systems for single-phase HVAC compressors. The company built its reputation on the EasyStart line of soft starters, which reduce the electrical strain a compressor places on its power source when it starts up.
Micro-Air's products serve RV owners, marine vessel operators, residential homeowners, and commercial HVAC installations, with manufacturing based in the United States.
Product Lines
SupplyHouse carries Micro-Air's EasyStart soft starters alongside the brand's control and monitoring hardware. The EasyStart line reduces compressor startup strain. This lets an air conditioner run on a limited power source, such as a generator, inverter, or reduced-capacity utility connection, when it otherwise couldn't start.
EasySurge Guardian adds surge protection for home HVAC systems, while the EasyTouch RV thermostat brings Wi-Fi and Bluetooth remote monitoring to RV climate control. Marine control systems, including control boards, displays, sensors, and pump relays, round out the catalog for boat owners and marine technicians.
Why Contractors Specify Micro-Air
Contractors specify Micro-Air's EasyStart soft starters when a customer's power source can't handle the inrush current of a compressor starting at full load. This is a common issue with portable generators, smaller inverters, or aging electrical service. Reducing that startup strain lets the compressor run on power sources it otherwise couldn't, which matters for RV and marine installations running on generator or inverter power.
For residential jobs, EasySurge Guardian gives contractors a way to add surge protection to an HVAC system. Micro-Air also manufactures its products in the United States.
How to Choose Micro-Air Products
Choosing the right Micro-Air soft starter starts with matching the EasyStart model to the compressor's horsepower and the power source it needs to run on. That source may be a generator, inverter, or standard utility circuit. RV and marine installations should confirm the EasyStart model is rated for the specific compressor and voltage found in that unit before installation.
For residential surge protection, contractors should size the EasySurge Guardian to the electrical service it's protecting. Marine control system components, such as control boards and displays, need to match the vessel's existing wiring and sensor setup to function correctly.
Frequently Asked Questions
What does a Micro-Air EasyStart soft starter do?
An EasyStart soft starter reduces the startup strain a compressor places on its power source. This lets the unit run on a generator, inverter, or reduced-capacity connection it otherwise couldn't start on.
Is Micro-Air EasyStart only for RVs?
No, EasyStart soft starters are used in RV, marine, and residential and commercial HVAC installations.
Does Micro-Air make surge protection products?
Yes, the EasySurge Guardian is Micro-Air's surge protector for home HVAC systems.
Where does Micro-Air manufacture its products?
Micro-Air manufactures its products in the United States.
Does Micro-Air's RV thermostat support remote monitoring?
Yes, the EasyTouch RV thermostat brings Wi-Fi and Bluetooth remote monitoring to RV climate control.