RoughinBox is a rough-in installation system for wall-mounted minisplit and VRF evaporator units, manufactured by MarketAir, Inc. MarketAir was founded in 1986 and is headquartered in Edison, New Jersey, where it operates as an importer, exporter, manufacturer, and distributor of HVACR installation components.
MarketAir builds its business around ducted, ductless, and VRF/VRV installation accessories. It distributes through manufacturer representatives and wholesale channels across the United States and Canada. RoughinBox is one of the company's core product lines, developed specifically for contractors installing wall-mounted minisplit and VRF systems.
Product Lines
On SupplyHouse, the RoughinBox line covers rough-in boxes sized for wall-mounted minisplit and VRF evaporator coil installations. They are built to fit standard wall cavities before the evaporator unit goes in. The boxes hold linesets, condensate drain lines, and low-voltage control wiring in place during framing, drywall, and paint. Those connections stay protected and organized until the unit is mounted.
MarketAir also produces the RD Series lineset enclosure and the SpeedStick WaterSwitch. These are two other installation accessories from the same company. Contractors sometimes specify them alongside RoughinBox on ductless and VRF jobs.
Why Contractors Specify RoughinBox
Wall-mounted minisplit and VRF jobs often have multiple trades working the same wall cavity before the evaporator unit is set. RoughinBox gives the lineset, drain, and wiring connections a fixed, protected location early in the job. Drywall and paint crews can then finish their work without disturbing or damaging those connections.
The box is set during rough-in, and the evaporator is mounted later. Contractors can sequence a job around other trades without re-opening a wall or re-routing a lineset that got buried or bent out of position. That reduces rework tied to coordinating minisplit and VRF installs with general construction schedules.
How to Choose RoughinBox Products
Start with the wall construction, since RoughinBox is built for standard stud spacing and needs a cavity depth that matches the model selected. Confirm the evaporator unit's lineset and drain port locations before picking a box. The box needs to line up with where those connections will exit the wall once the unit is mounted.
Condensate drain routing matters as much as lineset placement. Check whether the job calls for a horizontal or vertical condensate discharge path. Confirm the box supports the routing the site requires before it gets set into the wall. Correcting drain orientation after drywall is far more disruptive than catching it at rough-in.
Frequently Asked Questions
What is a RoughinBox used for?
It's a rough-in enclosure for wall-mounted minisplit and VRF evaporator installations. It holds the lineset, condensate drain, and control wiring in a fixed spot in the wall cavity. Other trades can finish framing, drywall, and paint before the evaporator unit is mounted.
Who manufactures RoughinBox?
RoughinBox is manufactured by MarketAir, Inc., an HVACR installation components company founded in 1986 and based in Edison, New Jersey. MarketAir also makes other ductless and VRF installation accessories. These include the RD Series lineset enclosure and the SpeedStick WaterSwitch.
What should I check before choosing a RoughinBox?
Start with the wall construction. RoughinBox is built for standard stud spacing and needs a cavity depth that matches the model selected. Then confirm the evaporator unit's lineset and drain port locations, so the box lines up with where those connections will exit the wall.
When should RoughinBox go into a wall during a job?
It goes in during rough-in, before drywall, so the lineset, drain, and wiring are protected and positioned correctly ahead of the evaporator unit being mounted later in the project.
Why does condensate drain routing matter when choosing a RoughinBox?
Drain orientation needs to be set correctly at rough-in. Check whether the job calls for a horizontal or vertical condensate discharge path. Confirm the box supports that routing before it is set into the wall, since correcting it after drywall is far more disruptive.