ScaleBlaster was launched in 1995 by Clearwater Enviro Technologies, a company founded in 1989 and headquartered in Largo, Florida. The brand manufactures electronic water conditioners marketed as a salt free and chemical free alternative to traditional water softeners.
Products are engineered, designed, and assembled in the United States. They are distributed through dealers, manufacturer reps, and retail stores across more than 70 countries.
Product Lines
ScaleBlaster's electronic water conditioners use electronic conditioning rather than chemical treatment or salt based ion exchange. They prevent new limescale from forming and help dissolve existing scale in pipes and equipment. Because the units do not backwash or discharge wastewater, they avoid the brine discharge associated with traditional salt based softeners.
The lineup covers residential models sized for individual homes. It also includes commercial and industrial models built for hotels, restaurants, hospitals, HVAC systems, cooling towers, agricultural operations, mining, and power plants.
Why Contractors Specify ScaleBlaster
Plumbers and facilities contractors specify ScaleBlaster on jobs where a homeowner or building owner wants scale control without the ongoing maintenance of a salt based softener. The units need no salt refills, no brine tank, and no backwashing cycle.
On commercial and industrial jobs, eliminating the wastewater discharge of a traditional softener also simplifies drainage requirements. This matters on sites where adding a floor drain or waste line for backwash water is not practical.
How to Choose ScaleBlaster Products
Selecting between ScaleBlaster's residential and commercial or industrial lines starts with pipe size and water volume. A single family home typically calls for a residential model sized to the main water line. A commercial building, cooling tower, or industrial process line needs a unit rated for higher flow and larger pipe diameters.
ScaleBlaster units work through electronic conditioning applied to the pipe rather than a plumbed inline cartridge. Confirm the unit's compatible pipe material and diameter range before ordering to make sure it mounts correctly on the intended line.
Frequently Asked Questions
Does a ScaleBlaster unit use salt like a traditional water softener?
No. ScaleBlaster uses electronic conditioning instead of salt based ion exchange, so there is no brine tank or salt to refill.
Where is ScaleBlaster manufactured?
ScaleBlaster products are engineered, designed, and assembled in the United States by Clearwater Enviro Technologies, based in Largo, Florida.
Can ScaleBlaster be used on commercial and industrial systems, not just homes?
Yes. ScaleBlaster makes commercial and industrial models for hotels, restaurants, hospitals, HVAC systems, cooling towers, agricultural operations, mining, and power plants, in addition to residential units.
Does a ScaleBlaster unit produce any wastewater?
No. ScaleBlaster units do not backwash or discharge wastewater, unlike traditional salt based softeners.
When was ScaleBlaster introduced?
ScaleBlaster was launched in 1995 by Clearwater Enviro Technologies, which was founded in 1989.