Super Lube traces back to 1980, when Sal and Hilda Randisi founded Synco Chemical Corporation. The Super Lube brand itself launched in 1986, and the company has been ISO 9001 certified since 1996.
The company manufactures premium synthetic lubricants, including food grade formulations, and its products are made in the United States.
Product Lines
Super Lube's catalog spans five categories. Greases include multi purpose, high temperature, silicone, O-ring, and railroad grades. Oils include gear, air tool, low temperature, and multi use synthetic formulations. Aerosols come in multi purpose, silicone, and dri film versions. Corrosion inhibitors include anti seize and metal protectant products. Specialty items include fire resistant hydraulic fluid and heat sink compound.
Products are used across eleven industries. These include transportation, heavy industry, hardware, marine, and agriculture. Others include food and beverage, plus mining and construction. Energy and utilities are also served.
Why Contractors Specify Super Lube
Contractors who need a lubricant that will not contaminate potable water or food contact surfaces specify Super Lube. Several of its formulations are food grade. That matters on jobs involving water heaters, food service equipment, or potable water fixtures, where a standard petroleum based lubricant is not appropriate.
The brand's ISO 9001 certification, held since 1996, also gives contractors a documented quality standard to point to on jobs that call for a lubricant meeting a formal specification.
How to Choose Super Lube Products
Choosing between Super Lube's grease, oil, and aerosol lines starts with the application. Threaded fittings and valve stems typically call for a grease formulation. Moving mechanical parts often do better with an oil. Hard to reach spots benefit from an aerosol that can be sprayed directly into the assembly.
For jobs touching potable water or food contact surfaces, confirm the product is food grade before use. Not every Super Lube formulation in the catalog carries that rating.
Frequently Asked Questions
Is Super Lube food grade?
Some Super Lube formulations are food grade synthetic lubricants. Not every product in the catalog carries that rating, so check the specific product before use on food contact surfaces.
When was Super Lube founded?
Super Lube traces back to 1980, when Sal and Hilda Randisi founded Synco Chemical Corporation. The Super Lube brand launched in 1986.
Is Super Lube ISO certified?
Yes. Super Lube has held ISO 9001 certification since 1996.
What product categories does Super Lube offer?
Super Lube's catalog covers greases, oils, aerosols, corrosion inhibitors, and specialty products such as fire resistant hydraulic fluid and heat sink compound.
Is Super Lube made in the United States?
Yes. Super Lube products are made in the United States.