Tuff-Stuff is manufactured by Innovative Energy Inc., a company based in Crown Point, Indiana that produces insulation and moisture barrier products made in the USA. The Tuff-Stuff line was developed to address a common jobsite problem: ground moisture and heat loss beneath concrete slabs.
Rather than treating vapor barriers and under-slab insulation as separate purchases, Innovative Energy built Tuff-Stuff as a combined product. This has made it a recognizable name among contractors pouring slabs over radiant systems or in below-grade construction.
Product Lines
The core Tuff-Stuff product is a thermal moisture barrier built from two layers of high-strength polyethylene bubble film. It is sold on SupplyHouse in roll sizes including 48 inches by 125 feet and 72 inches by 125 feet.
The material is rated for water vapor transmission of 0.002 per ASTM E96 and puncture resistance greater than 500 PSI per ASTM F1306. Its thermal resistance is R-1.16 per ASTM C518, and its compression strength is 101 psf at 10 percent compression. This gives it a defined technical profile for use under heated or unheated concrete slabs.
Why Contractors Specify Tuff-Stuff
Pouring concrete directly over unprotected ground invites moisture migration and heat loss that can undermine a radiant slab's performance for the life of the building. Tuff-Stuff addresses both issues in a single install step, which simplifies the sequence for crews working under time pressure before a pour.
Its puncture resistance rating also matters on active jobsites, where rebar, tools, and foot traffic can damage lighter barrier materials before the concrete ever goes down. A rating above 500 PSI gives contractors more confidence that the barrier will still be intact at pour time.
How to Choose Tuff-Stuff Products
Roll size should be matched to the slab footprint and the number of seams a crew is willing to tape or overlap. The 72 inch by 125 foot roll covers more ground per roll on larger pours. The 48 inch width can be easier to handle in tighter spaces or smaller residential jobs.
For radiant slab work specifically, the R-1.16 thermal resistance value should be weighed against the overall insulation plan for the floor system. Tuff-Stuff is designed to work as part of a larger under-slab strategy rather than as the sole insulation layer in every climate.
Frequently Asked Questions
Does Tuff-Stuff replace the need for a separate vapor barrier under a slab?
Tuff-Stuff is built as a combined vapor barrier and insulation layer, with a water vapor transmission rating of 0.002 per ASTM E96, so it is designed to serve both functions in a single install.
What roll sizes are available for larger commercial pours?
SupplyHouse carries Tuff-Stuff in 48 inch by 125 foot and 72 inch by 125 foot rolls. The wider roll reduces the number of seams needed on larger slab areas.
Can Tuff-Stuff be installed under a radiant heat slab?
Yes, Tuff-Stuff is rated for use under heated or unheated concrete slabs and carries an R-1.16 thermal resistance rating per ASTM C518.
How does Tuff-Stuff hold up to jobsite abuse before the pour?
The material carries a puncture resistance rating above 500 PSI under ASTM F1306. It also has a compression strength of 101 psf at 10 percent compression. This supports typical rebar and foot traffic exposure before concrete is placed.
What is Tuff-Stuff made of?
Tuff-Stuff is a thermal moisture barrier built from two layers of high-strength polyethylene bubble film. It is made in the USA by Innovative Energy Inc.