Water Heater Handler is a manufacturer of water heater installation and removal tools for plumbing contractors and installers. The tools are produced by Summit Ridge Tool Company in Austin, Texas. The flagship product, the Water Heater Handler, is a handle system that attaches to the 3/4-inch inlet or outlet threaded nipple of residential water heaters. It allows one person to safely hand-carry an empty tank without assistance. The tool is designed specifically for attic and basement installations. In these locations, tight quarters and stairway access make standard hand-carrying of a water heater difficult and unsafe. Plumbing contractors and installers specify Water Heater Handler products for residential gas and electric tank water heater replacement. They are used where the installation location creates a one-person carrying challenge.
Product Lines
The Water Heater Handler (Model 64910)
The Water Heater Handler (SKU 64910) is the primary product in the Summit Ridge Tool Company catalog. The handle threads directly onto the 3/4-inch NPT inlet or outlet nipple on a residential water heater tank without additional tools. It distributes the empty tank's weight to a single ergonomic carrying point. Produced in orange, the Water Heater Handler is designed for use with empty residential gas and electric water heater tanks across standard residential sizes.
Attic Installation Applications
The Water Heater Handler's primary application is water heater replacement in attic installations, where the tank must pass through an attic access hatch and navigate across attic floor joists. The single-point handle gives the installer controlled maneuvering through confined spaces. Without a purpose-built carrying handle, attic water heater replacement typically requires two people due to the awkward shape of an empty tank in a confined space.
Basement and Mechanical Room Applications
The Water Heater Handler is also specified for basement, mechanical room, and crawl space installations. In these spaces, stairs, low clearances, or tight doorways can make standard hand-carrying of an empty tank difficult. The tool's thread-on attachment is compatible with the 3/4-inch NPT connections standard on residential gas and electric water heater inlet and outlet ports. It converts a difficult two-person job into a controlled one-person carry.
Why Contractors Specify Water Heater Handler
Water Heater Handler products are produced by Summit Ridge Tool Company in Austin, Texas for the installation and replacement conditions plumbing contractors encounter on residential water heater jobs. The thread-on design requires no modification to the water heater and no additional hardware. Attic and basement water heater replacements are among the most physically demanding single-trade tasks in residential plumbing service. The Water Heater Handler converts a two-person improvised carry into a controlled one-person operation.
Frequently Asked Questions
Where are Water Heater Handler products manufactured?
Water Heater Handler products are manufactured by Summit Ridge Tool Company in Austin, Texas.
What color is the Water Heater Handler Model 64910?
The Water Heater Handler (Model 64910) is produced in orange.
What type of water heater connection does the Water Heater Handler attach to?
The Water Heater Handler (Model 64910) attaches to the 3/4-inch inlet or outlet threaded NPT nipple on the top of a residential water heater tank. The thread-on design is compatible with standard 3/4-inch NPT connections on residential gas and electric water heater inlet and outlet ports.
Can the Water Heater Handler be used on a full water heater tank?
The Water Heater Handler is designed for use with empty residential water heater tanks only. Full or partially full tanks exceed safe single-person hand-carrying weight limits and shouldn't be moved with any single-point handle system.
Is the Water Heater Handler compatible with both gas and electric water heaters?
The Water Heater Handler is compatible with standard residential gas and electric tank water heaters that have accessible 3/4-inch NPT threaded nipples. Compatibility depends on the nipple being accessible and free of corrosion or obstruction.
What water heater installation scenarios is the Water Heater Handler designed for?
The Water Heater Handler is designed for attic and basement water heater replacement scenarios where tight access, stairways, hatch openings, or confined spaces make standard two-person hand-carrying difficult. The tool allows a single installer to carry an empty residential water heater through the access route by threading the handle onto the existing 3/4-inch nipple.