AquaGuard LLC manufactures the WAGS valve, a mechanical water heater safety shutoff device sold under the Aquaguard name. It is marketed as the original and only fully mechanical water and gas safety shutoff valve on the market since 2002. The product is Made in USA. It addresses a narrow but consequential problem: catching a leaking water heater before it causes serious water damage or, on gas-fired units, a gas safety hazard.
Aquaguard's core market is residential and light commercial water heater installations where a secondary layer of leak protection is wanted beyond a standard drip pan alone. Because the valve requires no external power supply, it functions independently of a building's electrical system, an advantage in a leak scenario where power may already be compromised.
Product Lines
The WAGS valve line centers on models built for different water heater configurations. The WAGS7200-5WG shuts off both the cold water supply and the gas supply, so it suits gas-fired water heaters. The WAGS7200-4W is a water-only shutoff for installations, such as electric water heaters, that don't need a gas cutoff.
Both models use the same core mechanism: a spring-loaded piston sitting in the water heater's drip pan. It activates once leaking water accumulates to a set depth. The valve then closes the applicable supply lines and displays a red indicator tab to show it has triggered.
Why Contractors Specify Aquaguard
Contractors specify the Aquaguard WAGS valve because it's a single-use mechanical safeguard. It doesn't depend on batteries, a control board, or a network connection to function. That matters on a leak-detection device that may sit dormant for years before it's called on to act. The valve's fully mechanical operation also simplifies the sales conversation. This helps with a customer who wants leak protection but isn't interested in maintaining smart-home sensors or replacing batteries on a schedule.
Aquaguard markets the WAGS valve as the original design in its category since 2002. Contractors get a long track record to point to rather than a newer, less-proven alternative. The dual water-and-gas shutoff option is also a meaningful selling point on gas-fired water heater replacements, where a leak carries both a water damage and a combustion safety dimension.
How to Choose Aquaguard Products
Start by confirming whether the water heater being protected is gas-fired or electric. That determines whether the WAGS7200-5WG's combined water-and-gas shutoff is needed or whether the water-only WAGS7200-4W is the correct fit. Verify the drip pan dimensions and connection sizing match the valve's installation requirements before ordering. The valve installs inline with the water heater's cold water supply and sits within the pan itself.
Because the valve is a single-use, non-resettable device, plan for replacement after any activation event rather than expecting the same unit to reset and continue protecting the installation. On gas-fired installations, coordinate the valve's gas shutoff function with local code requirements for gas safety devices before finalizing the installation.
Frequently Asked Questions
What is a WAGS valve?
It's a mechanical water heater safety shutoff device that sits in the drip pan beneath a water heater. When it detects a leak, it shuts off the water supply. On some models it also shuts off the gas supply.
What's the difference between the WAGS7200-5WG and WAGS7200-4W?
The WAGS7200-5WG shuts off both water and gas supply for gas-fired water heaters, while the WAGS7200-4W is a water-only shutoff for installations that don't need a gas cutoff.
Does the Aquaguard WAGS valve need batteries or power?
No, the valve is fully mechanical and requires no external power supply, so it keeps working even if electrical power is interrupted.
Can a WAGS valve be reset and reused after it activates?
No, it's a single-use, non-resettable device, so a triggered valve needs to be replaced rather than reset.
How long has the WAGS valve been on the market?
Aquaguard markets it as the original and only fully mechanical water and gas safety shutoff valve on the market since 2002.