Green Drain makes waterless trap seal devices that install into floor drains to block sewer gas, pests, and odors from entering a building when the drain's water trap dries out. The brand's products carry certifications in the United States, the European Union, Australia, and Denmark. This reflects a product line built for both domestic and international plumbing codes.
Green Drain's core markets include healthcare facilities, restaurants and hospitality venues, K-12 schools, commercial offices, industrial warehouses, and food manufacturing plants, along with residential use. These are largely spaces where floor drains sit unused for long stretches between water events. That is exactly the condition that causes a traditional trap seal to evaporate and lose its ability to block sewer gas.
Product Lines
The Green Drain lineup is built around a single mechanism, a one-way silicone valve. It is sized into four models to match common floor drain diameters. The GD2 suits residential and light commercial use. The GD3 suits commercial and healthcare settings. The GD4 suits general commercial applications. The GD6 suits industrial and heavy commercial drains.
Each model installs directly into an existing floor drain without tools. It sits below the strainer to seal the drain line while allowing full water flow when the drain is used. Because the entire line is variations on drain diameter rather than separate technologies, choosing a model mostly comes down to matching the trap seal to the drain opening size.
Why Contractors Specify Green Drain
Floor drains in mechanical rooms, break rooms, and rarely used commercial spaces are a known source of sewer gas complaints once the water trap evaporates. Re-priming a trap manually is not a permanent fix in low-use areas. A waterless trap seal removes that maintenance cycle. Facility managers and plumbing contractors often add Green Drain devices to drains with a history of dry-trap odor complaints.
In healthcare and food service settings, the one-way valve design also matters for infection control and pest exclusion. An open or dried-out trap can be a path for sewer gas, insects, and aerosolized contaminants to move between spaces. Green Drain's own testing reports retaining more than 99.9 percent of an aerosolized viral surrogate used to model that risk.
How to Choose Green Drain Products
Measure the floor drain opening first, since Green Drain's four models are differentiated primarily by size rather than feature set. The GD2 fits smaller residential and light commercial drains. The GD3 and GD4 cover most standard commercial and healthcare installations. The GD6 is sized for larger industrial drains.
Consider the drain's usage pattern as well. Drains that see infrequent water flow are the strongest candidates for a waterless trap seal. Examples include drains in mechanical rooms, storage areas, or seasonal-use spaces. Those are exactly the conditions that dry out a conventional water trap and let sewer gas escape into occupied space.
Frequently Asked Questions
How does a Green Drain trap seal work without water?
It uses a one-way silicone valve that stays closed to block sewer gas and odors. The valve opens to allow water through whenever the drain is used. This means it does not depend on a water trap staying full.
Which Green Drain model fits a standard commercial floor drain?
The GD3 and GD4 are sized for most commercial and healthcare floor drains. The GD2 fits smaller residential and light commercial drains. The GD6 is built for larger industrial openings.
Do Green Drain devices require any tools to install?
No. Each model installs into an existing floor drain without tools, sitting below the strainer.
Is Green Drain approved for use outside the United States?
Yes, Green Drain products carry certifications in the United States, the European Union, Australia, and Denmark.
Why would a floor drain need a waterless trap seal instead of a standard trap?
Floor drains that go long periods without water flow are prone to their trap seal evaporating, which opens a path for sewer gas and pests. A waterless trap seal stays sealed regardless of how often the drain is used.