Apply to be a TradeMaster!
Main product image of Hose Bibb Mounting Plate, 5-3/4" x 2-3/4" x 1/8"
Magnifying glass
Hover image to zoom

Hose Bibb Mounting Plate, 5-3/4" x 2-3/4" x 1/8"

SKU:
HBMP
Rating:
(53)
Q&A:
(0)
Hose Bibb Mounting Plate, 5-3/4" x 2-3/4" x 1/8"
Magnifying glass
Hover image to zoom
$14.15 each
In Stock
In Stock
Get 155 Tue, Nov 3
Order by today, receive Tuesday
Free Shipping On orders over $99
Easy Returns No restocking fee for 90 days

Description

–
The Mounting Plate provides a neat and attractive solution to a common problem when installing sillcocks. It makes the job easier, faster and more satisfying. Plumbers and Homeowners love them.
  • Hose Bibb Mounting Plate prevents drafts, moisture, insects and vermin from entering the building through gaps between the hose bibb and the outside wall.
  • Holds hose bibb securely so as to prevent stresses on plumbing.
  • Assures the proper pitch on frost-proof hydrants and saves time on installation.
  • Neat, attractive and a professional appearance to a common problem of the plumbing field.
  • Dimensions: 5-3/4" x 2-3/4" x 1/8"
  • Between the outer set of screw holes is 2-3/8"
  • Between inner set of screw holes is 1-5/8"
  • From outer to opposite side inner hole is 2".

Specs

–
Product Type:

Mounting Plate

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


QUICK SUPPORT

Order StatusShipping PolicyReturnsIs My Item in Stock?Request Item for Site

You May Also Need

10", 1/2" MIP x 1/2" Inside Sweat Frost-Free Anti Siphon Sillcock (Lead Free)
SKU: SK050MC-10AS
Bluefin

Product Reviews

4.51 out of 53 reviews
89% would recommend this product
4.51
out of 53 Reviews
89% would recommend this product
WRITE A REVIEW
5 star
77%
4 star
9%
3 star
6%
2 star
2%
1 star
6%
WRITE A REVIEW
Customer Images

Most Liked Positive Review

Best price for this product I could find.

I specifically looked for something like this because the old bibb had worn away the holes, so I wanted to secure it in new holes. Used anchor sleeves and it was tight. Sillcock set screws worked but it took some effort, but the design is nice and it looks nice. I put some construction adhesive behind it and some silicone around it.
VS

Most Liked Negative Review

Can't Mount any Hose Bibbs

I bought this trying to make it easier for mounting my 2 new hose bibbs. The ones I bought through supply house didn't fit and neither did any of the once from the hardware stores. There are 4 holes to mount and ones set is too narrow and the other is too wide.
Showing 1-10 of 53 reviews

Hose bib back plate

I used this plate to secure a hose bib on a metal building. Product work perfectly.
MPagg
Dublin, TX
1 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

A must buy!

I always order the mounting plate when installing the Prier quarter turn wall hydrant. It makes installation a breeze and the hydrant is mounted solid as a rock!
Berkley
Winston Salem
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Super Reinforcer for Reliable Bibbs

I placed a Mounting Plate at each of my outside bibbs. Everyone knows not to tug on an attached garden hose, but it happens. Also, to further support the end of the pipe run terminating at the bibb, I elected to use the mounting plate so that the bibb's cast ears could be secured to the plate with machine screws, while the mounting plate tabs were secured to the composite plinth with lags. In that way the mounting plate provides a transition that allows all those materials to be engaged with the appropriate fasteners.
RodNJ
NJ
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

I would buy this again and again

Always top quality items with extremely fast delivery! Doesn't get any better! Thanks!
Conway
Newburgh, NY
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

It worked fine. Would purchase again, if needed.

I used this product to hook up an outside hose connection to our indoor plumbing.
N/A
Abington, PA
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

YES

THE THREADED HOLES WOULD NOT LINE UP WITH SILL COCK HOLES. PLATE IS WELL MADE ! MAYBE SHOULD CHECK WITH SUPPLY HOUSE TO SEE IF THIS PLATE WILL FIT THE SILLCOCK YOU ARE LOOKING AT.
BOOKIE
MA
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Love this thing

No more fighting trying to get anchors in!
Bob the plumber
Stony Point NY
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

I would recommend this product

Good idea, always hard to secure replacement
BO
Staten island, ny
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

As easy to make one myself than to adapt this

It won't take a lot of bibbs. Screw holes are in the wrong place and interfere with drilling and tapping correct holes. The existing holes must be filled before proceeding. It's just a piece of aluminum. Would be better if they hadn't pre-drilled holes or at least specified the limitations of what they did. It isn't hard to do that.
water
VA
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

excellent product.

works great, a little pricey for what it is, but really solves the issue of securing a FF hose bibb when the masonry is crumbling.
tim
Denver, Pa
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy