Kibosh is a pipe repair clamp manufactured in the United Kingdom through a manufacturing partnership with Rothenberger. The clamp is designed to stop a leak on a burst or accidentally perforated pipe within seconds, even while water is still flowing. The pipe keeps functioning under pressure until a permanent repair can be made.
Trade professionals such as plumbers, electricians, builders, and maintenance staff use the clamp as an emergency stopgap. It suits a pipe that is accidentally punctured during other work, such as drilling or nailing.
Product Lines
The core Kibosh product is a reusable pipe repair clamp available in half inch and three quarter inch sizes. It is built to fit metal, plastic, and multilayer pipe, as well as some leaky fittings. The clamp is rated to withstand 10 bar of pressure, equal to about 150 psi, and works on both hot and cold water lines once installed.
Kibosh clamps are made from non-toxic materials. They are designed to be reusable rather than a single-use fix, so a contractor can carry one on a truck for repeat emergency calls instead of replacing it after each use.
Why Contractors Specify Kibosh
Plumbers and maintenance contractors keep a Kibosh clamp in the truck. It stops a leak in seconds without shutting down the whole system first, which buys time to schedule a proper repair instead of reacting to an active flood.
Because the clamp works on metal, plastic, and multilayer pipe, a single product covers most pipe materials a contractor runs into across older and newer construction. Separate repair parts for each pipe type are not needed.
How to Choose Kibosh Products
Sizing a Kibosh clamp comes down to matching the clamp diameter to the outer diameter of the damaged pipe. The clamp is available in half inch and three quarter inch sizes.
For a leaking fitting rather than a straight pipe run, confirm the clamp can seat fully around the fitting profile before relying on it as the repair. Once the clamp is off the pipe and the area is dry, it can be reused on a future call rather than treated as disposable.
Frequently Asked Questions
Can a Kibosh clamp be used on both metal and plastic pipe?
Yes. Kibosh clamps are built to work on metal, plastic, and multilayer pipe, as well as some leaky fittings.
What pressure rating does a Kibosh clamp handle?
Kibosh clamps are rated to withstand 10 bar of pressure, or about 150 psi.
Can a Kibosh clamp be installed while the pipe is still leaking?
Yes. The clamp is designed to clamp shut on a burst pipe within seconds, even while water is actively leaking.
Is a Kibosh clamp a permanent repair?
No. It is an emergency stopgap that lets the pipe keep functioning under pressure until a permanent repair is made.
Is a Kibosh clamp reusable?
Yes. The clamp is made from non-toxic materials and is designed to be reused rather than replaced after a single repair.