Suntec Industries was formed in 1984 through the acquisition of Sundstrand Corporation's hydraulic division, a business that had been producing oil burner pumps since 1934. The company runs two production sites: one near Dijon, France, and one in Glasgow, Kentucky, serving the North American market.
Suntec is ISO 9001 certified for quality management since 1993 and ISO 14001 certified for environmental management since 2012. The company employs around 150 people and exports about 97 percent of its production.
Product Lines
Suntec's core product lines are gear pumps and gas blocks for oil burners and fuel oil heating systems. The range spans more than 600 product references in liquid-fuel and gaseous-fuel categories. The lineup includes pumps compatible with biofuel blends up to B20, B30, B100, and HVO.
Beyond residential and commercial heating, Suntec pumps and mixers are used in industrial process heating, high-pressure cleaning equipment, marine heating systems, and vehicle heating. The company also makes hydrogen and natural gas mixers and compact micro-hydraulic components.
Why Contractors Specify Suntec
Heating technicians specify Suntec pumps in part because the company's product lineup already covers biofuel compatibility. About 71 percent of Suntec's products work with biofuel blends, which matters as more jurisdictions phase in biofuel requirements for heating oil. A technician replacing a failed pump on an older system may not need to source a separate biofuel-rated part.
The company has held ISO 9001 certification since 1993 and ISO 14001 certification since 2012. These give specifiers a documented quality and environmental management record for commercial or institutional jobs that require certified suppliers.
How to Choose Suntec Products
Selecting a Suntec pump starts with the fuel type and blend percentage the system runs on. Standard fuel oil systems can use the core gear pump line. Systems running biofuel blends should be matched to a pump rated for that specific blend, such as B20, B30, B100, or HVO, rather than assumed to be compatible.
For gas-fired equipment, Suntec's gas block line replaces older mechanical gas train components. The company's hydrogen and natural gas mixers apply to newer systems designed around alternative fuel blending rather than straight fuel oil or natural gas.
Frequently Asked Questions
When was Suntec Industries founded?
Suntec Industries was formed in 1984 by acquiring Sundstrand Corporation's hydraulic division, which had produced oil burner pumps since 1934.
Where does Suntec manufacture its products?
Suntec operates two production sites: one near Dijon, France, and one in Glasgow, Kentucky, which serves the North American market.
Are Suntec pumps compatible with biofuel heating oil?
Yes. About 71 percent of Suntec's products are biofuel-compatible, with pumps rated for blends including B20, B30, B100, and HVO.
Is Suntec ISO certified?
Suntec is ISO 9001 certified for quality management, held since 1993, and ISO 14001 certified for environmental management, held since 2012.
Does Suntec make anything besides oil burner pumps?
Yes. Suntec also manufactures gas blocks, compact micro-hydraulic components, and hydrogen and natural gas mixers. These serve heating and industrial applications.