Tribal is a US manufacturer of brass and steel machined fittings. It produces parts at two plants, in Marshall, Michigan, and Chesnee, South Carolina, with an additional facility in Kansas City, Missouri. Every fitting Tribal ships is made domestically, a point the company emphasizes across its OEM, custom, and shelf-line business.
Tribal fittings reach a wide span of industries beyond plumbing and HVAC. These include gas, propane, fluid power, hydraulic, marine, automotive, defense, medical, food and beverage, refrigeration, and oil applications. Such breadth reflects the company's core capability: high-volume precision machining rather than a single market niche.
Product Lines
Tribal's fitting range includes PEX fittings, gas and flare fittings, compression fittings, bulkhead fittings, and pipe thread fittings. These cover the connection types most common in plumbing and gas distribution work. Beyond assembled fittings, Tribal also produces custom machined parts in aluminum, brass, bronze, and other specialty metals and plastics for OEM customers.
Production runs through CNC mills and lathes, alongside multi-spindle screw machines such as Hydromats, Gnuttis, Davenports, and Acmes. This equipment supports forgings, castings, and turned parts up to three inches in diameter. Tribal fittings carry NSF, CSA, and ISO certification along with UL listing, depending on the product line.
Why Contractors Specify Tribal
Contractors specify Tribal fittings for jobs where domestic sourcing and certification matter, since the company machines every part at its US plants rather than importing finished components. NSF, CSA, and ISO certification on applicable product lines gives specifiers documentation they can point to on code-driven jobs.
Tribal's manufacturing base spans plumbing, HVAC, and gas applications. Contractors working in more than one trade can source PEX, gas, flare, and compression fittings from a single brand rather than juggling separate suppliers for each connection type.
How to Choose Tribal Products
Matching a Tribal fitting to the job starts with the connection type. Use PEX fittings for tubing runs, gas and flare fittings for fuel gas lines, and compression or bulkhead fittings for mechanical joints that need to be serviceable later. Material selection between brass and steel machined parts should follow the pressure, temperature, and corrosion exposure of the specific application.
For OEM or custom parts, buyers should confirm which certification applies to the specific part number needed. The certification may be NSF, CSA, ISO, or UL. It can vary by product line rather than applying uniformly across the entire Tribal catalog.
Frequently Asked Questions
Where are Tribal fittings manufactured?
Tribal manufactures its brass and steel fittings at plants in Marshall, Michigan and Chesnee, South Carolina, with an additional facility in Kansas City, Missouri.
What certifications do Tribal fittings carry?
Depending on the product line, Tribal fittings carry NSF, CSA, and ISO certification, and some are UL listed.
What connection types does Tribal offer?
Tribal produces PEX fittings, gas and flare fittings, compression fittings, bulkhead fittings, and pipe thread fittings.
Does Tribal only serve the plumbing trade?
No, Tribal fittings also serve HVAC, gas, propane, fluid power, hydraulic, marine, automotive, defense, medical, food and beverage, refrigeration, and oil industries.
Can Tribal produce custom machined parts?
Yes, Tribal machines custom parts for OEM customers in aluminum, brass, bronze, and other specialty metals and plastics. These include forgings, castings, and turned parts up to three inches in diameter.