Flair builds smart home HVAC control products, including motorized vents, room sensors, and a hub-based control system. The products are marketed for trade professionals and homeowners looking to improve comfort in homes with central heating and cooling.
Flair's products work alongside existing HVAC equipment rather than replacing it. The company works as an official partner alongside several major thermostat platforms.
Product Lines
SupplyHouse carries Flair's Smart Vent line, motorized vents that install in place of standard floor, ceiling, or wall registers to regulate airflow room by room. Flair's Puck 2 and Puck 2 Pro serve as room sensors that feed temperature and occupancy data into the system. The Bridge and Bridge Pro act as the hub that coordinates the vents and sensors.
Flair's hvacOS software platform ties the hardware together. The company also offers zoning and air-balancing solutions for ducted systems. Other products include controls for ductless mini-splits and smart control add-ons for staged heating systems and electric baseboard heat.
Why Contractors Specify Flair
Contractors specify Flair on jobs where a customer has comfort complaints in specific rooms but doesn't want a full zoning system installed. The Smart Vent and Puck sensor combination can balance airflow without new ductwork or dampers. Flair is compatible with ecobee, Honeywell, Nest, Sensi, Carrier, and Bryant thermostats. It can often be added to a system that's already using one of those platforms without a full equipment change-out.
Working as an add-on rather than a full-system replacement makes Flair a practical fit for retrofit and comfort-complaint calls.
How to Choose Flair Products
Confirm which thermostat platform the home already uses before ordering Flair hardware, since compatibility and setup steps vary by connected system. For a single problem room, a Smart Vent and Puck sensor pair is often enough. A home with multiple comfort complaints across different rooms or floors may need the Bridge hub to coordinate several vents at once.
On ductless mini-split or staged heating systems, check which Flair control option is built for that specific equipment type before ordering. The standard Smart Vent line is designed for ducted forced-air systems.
Frequently Asked Questions
What does the Flair Smart Vent do?
The Flair Smart Vent is a motorized vent that installs in place of a standard floor, ceiling, or wall register and adjusts airflow to help balance temperature between rooms.
What thermostats work with Flair?
Flair works as an official partner with ecobee, Honeywell, Nest, Sensi, Carrier, and Bryant thermostats and systems, meaning those platforms are built to work directly with Flair's hardware.
What is the difference between the Flair Puck and Bridge?
The Puck is a room sensor that tracks temperature and occupancy, while the Bridge is the hub that coordinates multiple Smart Vents and Pucks across a home.
Can Flair be used with a ductless mini-split system?
Yes, Flair offers a control option built specifically for ductless mini-split systems, separate from its standard ducted Smart Vent line.
Does Flair replace a home's existing HVAC equipment?
No. Flair's products work alongside existing HVAC equipment such as the furnace, air handler, or mini-split system rather than replacing it.