GREE was founded in 1991 and has grown into the world's largest specialized air conditioner manufacturer, based in Zhuhai, China, with operations spanning more than 180 countries. The company's mini-split and central air systems reach residential and light commercial installations across North America through distributors including SupplyHouse.
Heavy investment in engineering backs the brand's size. GREE puts roughly 3 percent of its budget into research and development each year across a network of research institutes. The company also holds a large patent portfolio built up over three decades of compressor and refrigerant engineering. That scale lets GREE run multiple mini-split product lines in parallel rather than a single general-purpose unit.
Product Lines
SupplyHouse carries GREE's single-zone and multi-zone ductless mini split systems, along with mini split accessories and individual multi-zone indoor units sold separately from the outdoor condenser. The single-zone Sapphire Ultra line, for example, includes a 9,000 BTU heat pump package rated at 27 SEER2 and running on R-410A refrigerant.
Multi-zone systems use a single outdoor condenser, such as the Multi21+ line, paired with separate indoor units for each room. SupplyHouse sells these condensers and indoor heads as individual line items rather than fixed bundles. This lets a contractor size a system room by room. GREE's newer multi-zone condensers, including models like the MUL18HP230V1R32AO, have moved to R32 refrigerant rather than the R-410A used in older single-zone packages.
Why Contractors Specify GREE
Cost and lead-time pressure on ductless retrofit work pushes many contractors toward a manufacturer with deep production capacity. GREE is the largest dedicated air conditioner maker in the world, and that scale appeals to contractors working under those pressures.
DC inverter compressors across the GREE line adjust output continuously rather than cycling on and off. This keeps a room at a steadier temperature and cuts the compressor wear that comes with frequent full-power starts. Coil construction on the Sapphire Ultra units pairs copper tubing with aluminum fins finished for corrosion resistance. A 500-hour salt spray test verifies this finish, which matters for coastal or humid installations.
How to Choose GREE Products
Match BTU capacity to the room or zone being conditioned first. An undersized single-zone unit like the 9,000 BTU Sapphire Ultra will run constantly in a space too large for it. An oversized unit short-cycles and struggles with humidity control in a small room.
Refrigerant type is worth checking before mixing components. GREE's older single-zone packages run R-410A, while newer multi-zone condensers such as the Multi21+ line have shifted to R32. The two refrigerants aren't interchangeable within the same system. Single-zone jobs generally call for the simpler outdoor-to-indoor pairing. A home with several rooms that need separate control calls for a multi-zone condenser sized for the combined load of its indoor units.
Frequently Asked Questions
What refrigerant do GREE mini split systems use?
It depends on the line. Older single-zone packages like the Sapphire Ultra run on R-410A, while newer multi-zone condensers such as the Multi21+ have moved to R32.
How many indoor units can a GREE multi-zone system support?
That depends on the specific condenser model, since each one is rated for a maximum combined indoor capacity. SupplyHouse sells GREE's multi-zone condensers and individual indoor units separately, so a contractor selects each indoor head to fit within the outdoor unit's total rated capacity.
What does SEER2 mean on a GREE unit like the Sapphire Ultra?
SEER2 is a cooling-efficiency rating measured under a revised industry test standard; a higher number means better efficiency at cooling the space over a season. The 9,000 BTU Sapphire Ultra single-zone package, for example, carries a 27 SEER2 rating.
Are GREE mini split coils resistant to corrosion in coastal installations?
The Sapphire Ultra line's copper tube and aluminum fin coil is finished to pass a 500-hour salt spray test. Manufacturers use this standard test to demonstrate resistance to the salt-air corrosion common near coastlines.
Does GREE make anything besides ductless mini splits?
Yes. Beyond mini splits, GREE's catalog includes central air systems, packaged units, and PTAC equipment for commercial and light commercial applications. SupplyHouse's GREE catalog is focused on the mini split and accessory lines.