Irritrol has manufactured professional grade irrigation products since 1967, building a reputation among landscape contractors and irrigation specialists for durable valves and controllers. The company pioneered PVC jar top and glass filled nylon valve technology. These designs set new standards for reliability in underground irrigation systems and are still referenced across the industry today. Irritrol sells primarily through specialized irrigation distributors rather than general retail, a strategy that keeps the brand closely tied to the professional installer market it serves.
Contractors and property managers rely on Irritrol equipment for residential and light commercial irrigation systems, from single-zone lawn setups to multi-zone properties requiring centralized control. The company backs its products with a five-year warranty from the date of installation, reflecting confidence in long-term field performance across varying soil, water, and climate conditions.
Product Lines
Irritrol's valve lineup covers a range of flow, pressure, and installation requirements. The 2400/2600, 2500, and 2700 series cover standard in-line and angle valve configurations. The 205 and 311A series address specific flow and pressure regulation needs. The 100 and 100S series round out the valve lineup for smaller residential zones. The DZVK series and the Omnireg pressure regulator give installers options for pressure sensitive applications. The 2623DPR and 300 valve adapters support retrofit and replacement work on existing systems. The 200B and 700 series extend coverage into additional flow ranges.
Beyond valves, Irritrol also produces irrigation controllers, sensors, and spray and rotor heads that round out a full system. The Super Blue Flex tubing line supports flexible drip and micro-irrigation runs. The company's SMRT Logic platform extends control beyond irrigation alone, offering a single wireless interface for coordinating irrigation, lighting, water features, and pumps on the same property.
Why Contractors Specify Irritrol
Contractors specify Irritrol valves and controllers largely because the components are straightforward to install, service, and stock. Standardized valve series like the 2400/2600 and 2700 lines use consistent bodies and fittings across models. Crews familiar with one Irritrol product can move to another without relearning installation steps. That consistency also simplifies parts inventory for irrigation companies servicing multiple properties with different valve generations.
The brand's five-year product warranty gives contractors a longer callback window, reducing the risk of unpaid warranty labor on jobs completed years earlier. Irritrol sells through irrigation-focused distributors rather than general retail. Contractors also get access to technical support geared toward installation and troubleshooting rather than consumer-facing sales. This matters on more complex commercial or multi-zone jobs.
How to Choose Irritrol Products
Selecting the right Irritrol valve series starts with matching flow rate and pressure requirements to the specific zone being controlled. Smaller residential zones with limited flow typically pair well with the 100 or 100S series. Larger zones or commercial applications may call for the 2400/2600 or 2700 series and their higher flow capacity. Where water pressure varies significantly across a property, the Omnireg pressure regulator or DZVK series can help maintain consistent output at the sprinkler heads themselves.
Controllers should be sized to the number of zones on the property and the level of scheduling flexibility the job requires. For properties running irrigation alongside lighting or water features, the SMRT Logic platform is worth considering since it consolidates control into one wireless interface rather than running separate systems. When replacing or retrofitting older Irritrol valves, the 2623DPR and 300 adapters simplify matching new components to existing pipe and wiring without a full system rebuild.
Frequently Asked Questions
How long has Irritrol been making irrigation products?
Irritrol has manufactured professional grade irrigation products since 1967, with decades of history developing valve and controller technology for the landscape industry.
What warranty does Irritrol offer on its products?
Irritrol backs its products with a five-year warranty starting from the date of installation.
Which Irritrol valve series works best for small residential zones?
The 100 and 100S series are sized for smaller residential zones with lower flow requirements, making them a common choice for single-family lawn systems.
Can Irritrol controllers coordinate with other systems on a property?
Yes. Irritrol's SMRT Logic platform provides a single wireless interface that can coordinate irrigation alongside lighting, water features, and pumps on the same property.
What should I check before replacing an old Irritrol valve?
Confirm the flow rate and pressure requirements of the zone. Then check whether the 2623DPR or 300 valve adapters are needed to match new valve bodies to existing pipe and wiring.