Real People. Real Service.
Help Face
Need a little help?
Live Chat
: Online Now
Right sizing is the difference between steady comfort and wasted fuel. A boiler BTU calculator estimates hourly heating load so boiler output matches real demand. In short, it uses system type, heated square footage, location, home age, and renovation status to recommend a BTU range that guides equipment selection.
Oversized boilers short cycle, waste fuel, and wear out faster. Undersized boilers run constantly and still struggle in cold weather. A quick, building-specific BTU estimate helps avoid both outcomes.
Questions? View the Boiler FAQs below
Q1
Which best describes your heating system?
Heating system type
Q2
What is the square footage of your home (the area to be heated)?
Sq.ft.
Q3
Location: Please select the city closest to your home.
Q4
How old is your home?
Home age
Q5
Renovations: Have you made significant renovations to your home?
Home renovations
More Information
Why Boiler Sizing Matters
  • Energy efficiency: Output matches load instead of burning fuel in short bursts.
  • Comfort: Even temperatures hold during peak demand.
  • Lower operating costs: Fuel use aligns with actual need.
  • Longer service life: Fewer on-off cycles reduce wear.
What This Boiler Sizing Calculator Considers
  • System type: Low-temperature radiant heat or high-temperature emitters such as baseboard, fan coils, or radiators.
  • Heated square footage: Interior conditioned area only.
  • Location: State and nearest city reflect local design temperatures.
  • Home age: Construction era influences insulation and air sealing.
  • Renovations: Major upgrades often lower required BTU output.
The result is an estimated BTU per hour range suitable for shortlisting boiler models by size.
Typical BTU Ranges by Square Footage
Most buildings fall between 30 and 60 BTU per square foot, depending on climate and envelope quality.
  • Warm climates: about 30–35 BTU per sq ft
  • Moderate climates: about 40–50 BTU per sq ft
  • Cold climates: about 50–60 BTU per sq ft
The calculator adjusts within these bands using the inputs above.
Boiler FAQs
Is BTU the same as BTU/hr?
Not quite. A BTU is just the unit of heat energy. When you see a boiler rated in BTU per hour, that's how much heat it can actually deliver in an hour of run time.
How many BTU per square foot are typical?
Rule of thumb: figure 30–60 BTU per square foot. Newer, tighter homes land closer to 30. Drafty old places in cold climates? Closer to 60.
Why does system type change the size?
Because not all emitters play by the same rules. Radiant panels run cooler water than baseboards or radiators, so they need more surface area to hit the same comfort level. Water temperature + emitter type = the output you'll actually need.
How accurate is this compared to Manual J?
Manual J is the full deep-dive — an engineer's load calculation with all the details. This calculator is the quick version: fast, practical, and plenty accurate for most residential and light commercial jobs.
What happens if a boiler is oversized?
It short cycles, burns more fuel than it should, wears itself out faster, and leaves you with uneven heat. In other words: a bigger boiler isn't better.
What happens if a boiler is undersized?
It runs and runs but struggles to ever catch up. On the coldest days, comfort slips and rooms never quite reach temperature.
Does insulation or window quality matter?
Absolutely. A tighter envelope keeps more heat in, meaning you can get by with fewer BTUs. That's why the calculator factors in age and renovation status — because a drafty old house and a freshly updated one aren't in the same league.
We're Here To Help!
Est. wait: < 1 min
Est. wait: 1 min
Response by Fri
Response by Fri

Open Now:
8am 7:45pm EDT

Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm
Footer People Non TradeMasterFooter People Non TradeMaster
Give Us Feedback
We'd love to hear about your experience with us.
TAKE SURVEY
Subscribe for More
Stay in the know with top brands & product spotlights!
App Image
Download Our App!
Easier and faster shopping on our 340,000+ products.  SupplyHouse App