Polymer Adhesives manufactures duct sealants, adhesives, and silicone sealants used in HVAC installation and service work. The company is based in Mineral Wells, Texas. It focuses its product development on sealing and bonding materials for residential and commercial duct systems rather than a broader building products catalog.
Many Polymer Adhesives products are formulated to help systems meet LEED certification credits. This matters on commercial jobs, where sealant and adhesive choices feed directly into a project's sustainability documentation. The company's product range spans water-based and solvent-based formulations, giving contractors options depending on cure time, application method, and job-site conditions.
Product Lines
SupplyHouse carries Polymer Adhesives' core categories of duct sealants, adhesives, and silicone sealants. The Polymer Sealants line includes water and solvent-based duct sealant products such as Airseal 11 and Airseal 22, along with CADS formulations. These products seal duct seams and joints against air leakage. The Adhesives line includes Glasstack products such as Glasstack 25, Glasstack 35, and Glasstack 151. These commercial-grade adhesives come in water-based and solvent formulations. They bond duct insulation and related materials. Polymer Adhesives also supplies silicone sealants and accessories, including tapes used alongside its sealant and adhesive products.
Why Contractors Specify Polymer Adhesives
HVAC installers specify Polymer Adhesives products because duct sealing directly affects system efficiency and comfort complaints. A sealant that fails at a duct seam turns into a callback. Having water-based and solvent-based formulation options in the same product line lets a contractor pick the right cure time and application method for a given job. It also avoids switching manufacturers mid-project. On commercial work, the availability of LEED-credit-eligible formulations also gives contractors a straightforward way to support a project's sustainability requirements without researching a separate specialty product line.
How to Choose Polymer Adhesives Products
Selecting between Polymer Adhesives' sealant and adhesive lines starts with the specific joint or material being addressed. Duct seam sealing calls for a Polymer Sealants product like Airseal 11 or Airseal 22. Bonding insulation or other materials to ductwork calls for a Glasstack adhesive. Choosing between water-based and solvent-based formulations depends on job-site ventilation, drying time available, and any project specifications that call for low-VOC or LEED-eligible materials. Contractors working on commercial jobs with sustainability documentation requirements should confirm which specific product formulations qualify for LEED credits before specifying a sealant or adhesive for that scope.
Frequently Asked Questions
Where is Polymer Adhesives based?
Polymer Adhesives is headquartered in Mineral Wells, Texas.
What is the difference between Polymer Adhesives' sealants and its Glasstack products?
The Polymer Sealants line, including Airseal 11 and Airseal 22, is built for sealing duct seams and joints. Glasstack products such as Glasstack 25, Glasstack 35, and Glasstack 151 are adhesives used for bonding duct insulation and related materials.
Do Polymer Adhesives products qualify for LEED credits?
Many Polymer Adhesives formulations are designed to help projects meet LEED certification credits, which matters on commercial jobs with sustainability documentation requirements.
Does Polymer Adhesives offer both water-based and solvent-based products?
Yes. The product line includes water-based and solvent-based sealant and adhesive formulations. This gives contractors options based on cure time and job-site conditions.
What product categories does Polymer Adhesives manufacture?
Polymer Adhesives manufactures polymer sealants, adhesives, silicone sealants, and related accessories such as tapes for HVAC duct work.